DMA with PIT problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMA with PIT problem

Jump to solution
4,830 Views
wendersonolivei
Contributor IV

Hi all

 

I'm having a problem with DMA with PIT triggering. I've tried to config the TPM0 (CH0) timer to trigger the DMA, but it doesn't work; I always have a program break at PE_DEBUGHALT(); .

I was testing that because I want to use DMA to output a waveform at DAC, with a sample rate of the PIT. So, I've tried to do this:

 

#define SINUS_LENGTH 256  uint16_t Sinus[SINUS_LENGTH] = {         2047U,  2097U,  2147U,  2198U,  2248U,  2298U,  2347U,  2397U,  2446U,  2496U,  2544U,  2593U,  2641U,  2689U,         2737U,  2784U,  2830U,  2877U,  2922U,  2967U,  3012U,  3056U,  3099U,  3142U,  3184U,  3226U,  3266U,  3306U,         3346U,  3384U,  3422U,  3458U,  3494U,  3530U,  3564U,  3597U,  3629U,  3661U,  3691U,  3721U,  3749U,  3776U,         3803U,  3828U,  3852U,  3875U,  3897U,  3918U,  3938U,  3957U,  3974U,  3991U,  4006U,  4020U,  4033U,  4044U,         4055U,  4064U,  4072U,  4079U,  4084U,  4088U,  4092U,  4093U,  4094U,  4093U,  4092U,  4088U,  4084U,  4079U,         4072U,  4064U,  4055U,  4044U,  4033U,  4020U,  4006U,  3991U,  3974U,  3957U,  3938U,  3918U,  3897U,  3875U,         3852U,  3828U,  3803U,  3776U,  3749U,  3721U,  3691U,  3661U,  3629U,  3597U,  3564U,  3530U,  3494U,  3458U,         3422U,  3384U,  3346U,  3306U,  3266U,  3226U,  3184U,  3142U,  3099U,  3056U,  3012U,  2967U,  2922U,  2877U,         2830U,  2784U,  2737U,  2689U,  2641U,  2593U,  2544U,  2496U,  2446U,  2397U,  2347U,  2298U,  2248U,  2198U,         2147U,  2097U,  2047U,  1997U,  1947U,  1896U,  1846U,  1796U,  1747U,  1697U,  1648U,  1598U,  1550U,  1501U,         1453U,  1405U,  1357U,  1310U,  1264U,  1217U,  1172U,  1127U,  1082U,  1038U,  995U,   952U,   910U,   868U,         828U,   788U,   748U,   710U,   672U,   636U,   600U,   564U,   530U,   497U,   465U,   433U,   403U,   373U,         345U,   318U,   291U,   266U,   242U,   219U,   197U,   176U,   156U,   137U,   120U,   103U,   88U,    74U,         61U,    50U,    39U,    30U,    22U,    15U,    10U,    6U,     2U,     1U,     0U,     1U,     2U,     6U,         10U,    15U,    22U,    30U,    39U,    50U,    61U,    74U,    88U,    103U,   120U,   137U,   156U,   176U,         197U,   219U,   242U,   266U,   291U,   318U,   345U,   373U,   403U,   433U,   465U,   497U,   530U,   564U,         600U,   636U,   672U,   710U,   748U,   788U,   828U,   868U,   910U,   952U,   995U,   1038U,  1082U,  1127U,         1172U,  1217U,  1264U,  1310U,  1357U,  1405U,  1453U,  1501U,  1550U,  1598U,  1648U,  1697U,  1747U,  1796U,         1846U,  1896U,  1947U,  1997U };  void InitTimer(void) {   TPM0_SC = 0;    TPM0_CNT = 0;   TPM0_MOD = TPM_MOD_MOD(0xFFFF);   TPM0_C0V = TPM_CnV_VAL(0x1770);    TPM0_C0SC = (TPM_CnSC_CHIE_MASK | TPM_CnSC_MSA_MASK | TPM_CnSC_DMA_MASK);    TPM0_SC = (TPM_SC_CMOD(0x01) | TPM_SC_PS(0x00) | TPM_SC_DMA_MASK); //Set up clock and prescaler }  void InitMuxDMA(void) {   //Channel Configuration Register   DMAMUX0_CHCFG0 = DMAMUX_CHCFG_ENBL_MASK | DMAMUX_CHCFG_TRIG_MASK | DMAMUX_CHCFG_SOURCE(24); }  void InitDMA(void) {   //DMA Source Addr   DMA_SAR0 = (uint32_t)&Sinus[0];   //DMA Destination Addr   DMA_DAR0 = (uint32_t)&DAC0_DAT0L;   //DMA Status Register/ Byte Counter Register   DMA_DSR_BCR0 = DMA_DSR_BCR_BCR(256);   //DMA Control Register   DMA_DCR0 = DMA_DCR_ERQ_MASK | DMA_DCR_CS_MASK | DMA_DCR_SINC_MASK | DMA_DCR_SSIZE(0b10) | DMA_DCR_DINC_MASK | DMA_DCR_DSIZE(0b10);   //DMA Mux   InitMuxDMA(); }

 

Target: KL25Z

 

Can anyone help?

Original Attachment has been moved to: DMA-error-project-(FRDM-KL25Z).zip

0 Kudos
Reply
1 Solution
4,254 Views
BlackNight
NXP Employee
NXP Employee

I have not tried your example (PIT triggered), but I experimented with DMA and PWM. Maybe this helps:

http://mcuoneclipse.com/2014/06/07/tutorial-pwm-with-dma-on-armkinetis/

There is as well

First Adafruit NeoPixel Blinks with the FRDM Board | MCU on Eclipse

and

http://mcuoneclipse.com/2014/07/27/led-clock-with-kitchen-hot-pan-protector/

where I use DMA.

DMA code is in

mcuoneclipse/NeoPixel.c at master · ErichStyger/mcuoneclipse · GitHub

The Processor Expert Init component for DMA has a setting for PIT triggered DMA. When I tried this, I remember that worked as expected. So I think just something is missing in the settings.

View solution in original post

0 Kudos
Reply
6 Replies
4,254 Views
wendersonolivei
Contributor IV

BlackNight, I found what causes the unhandled exception. It was happening due a clk config missed. Thanks by the tip for ISR!

The code without exception:

void InitTimer(void)

{

  SIM_SCGC6 |= SIM_SCGC6_TPM0_MASK;

  TPM0_SC = 0;

  TPM0_CNT = 0;

  TPM0_MOD = TPM_MOD_MOD(0xFFFF);

  TPM0_C0V = TPM_CnV_VAL(0x1770);

  TPM0_C0SC = (TPM_CnSC_CHIE_MASK | TPM_CnSC_MSA_MASK | TPM_CnSC_DMA_MASK);

  TPM0_SC = (TPM_SC_CMOD(0x01) | TPM_SC_PS(0x00) | TPM_SC_DMA_MASK); //Set up clock and prescaler

}

void InitMuxDMA(void)

{

  //Channel Configuration Register

  SIM_SCGC6 |= SIM_SCGC6_DMAMUX_MASK;

  DMAMUX0_CHCFG0 &= ~DMAMUX_CHCFG_ENBL_MASK;

  DMAMUX0_CHCFG0 |= DMAMUX_CHCFG_TRIG_MASK;

  DMAMUX0_CHCFG0 |= DMAMUX_CHCFG_SOURCE(24);

  DMAMUX0_CHCFG0 |= DMAMUX_CHCFG_ENBL_MASK;

}

void InitDMA(void)

{

  //Init DMA Clock

  SIM_SCGC7 |= SIM_SCGC7_DMA_MASK;

  //DMA Source Addr

  DMA_SAR0 = (uint32_t)&Sinus[0];

  //DMA Destination Addr

  DMA_DAR0 = (uint32_t)&DAC0_DAT0L;

  //DMA Status Register/ Byte Counter Register

  DMA_DSR_BCR0 = DMA_DSR_BCR_BCR(256);

  //DMA Control Register

  DMA_DCR0 = DMA_DCR_ERQ_MASK | DMA_DCR_CS_MASK | DMA_DCR_SINC_MASK | DMA_DCR_SSIZE(0b10) | DMA_DCR_DINC_MASK | DMA_DCR_DSIZE(0b10);

  //DMA Mux

  InitMuxDMA();

}

But, anyway, the DMA wasn't handled the DAC. Someone knows why?

4,255 Views
BlackNight
NXP Employee
NXP Employee

I have not tried your example (PIT triggered), but I experimented with DMA and PWM. Maybe this helps:

http://mcuoneclipse.com/2014/06/07/tutorial-pwm-with-dma-on-armkinetis/

There is as well

First Adafruit NeoPixel Blinks with the FRDM Board | MCU on Eclipse

and

http://mcuoneclipse.com/2014/07/27/led-clock-with-kitchen-hot-pan-protector/

where I use DMA.

DMA code is in

mcuoneclipse/NeoPixel.c at master · ErichStyger/mcuoneclipse · GitHub

The Processor Expert Init component for DMA has a setting for PIT triggered DMA. When I tried this, I remember that worked as expected. So I think just something is missing in the settings.

0 Kudos
Reply
4,254 Views
wendersonolivei
Contributor IV

I got that with your DMA and PWM example. Thanks!

0 Kudos
Reply
4,254 Views
BlackNight
NXP Employee
NXP Employee

To know which interrupt was raised, could you enable 'own for every' in the Processor Expert CPU build tab settings?

See Oh my! An Interrupt… | MCU on Eclipse

That way we would know at least what interrupt is firing.

Erich

4,254 Views
wendersonolivei
Contributor IV

Hi Erich!

Thanks, it's really helpful (not only for this project).

Well, now I know that is a Cpu_ivINT_Hard_Fault isr, and this is happening when I try to write the DMAMUX0_CHCFG0. Do you know why a write occurrence on this reg is generating this error?

0 Kudos
Reply
4,254 Views
BlackNight
NXP Employee
NXP Employee

Looks you already identified the spot what caused the hard fault.

Just in case, if not seen these:

http://mcuoneclipse.com/2012/11/24/debugging-hard-faults-on-arm-cortex-m/

and for Processor Expert there is even a dedicated component:

http://mcuoneclipse.com/2012/12/28/a-processor-expert-component-to-help-with-hard-faults/

This helps with debugging hard faults.

Erich

0 Kudos
Reply