DMA question. What is the differences between MLNO vs MLOFFNO vs MLOFFYES

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMA question. What is the differences between MLNO vs MLOFFNO vs MLOFFYES

Jump to solution
2,542 Views
nijo
Contributor II

Hey,

 

Could anyone help me with the difference between then these fields:

 

DMA_TCD0_NBYTES_MLNO
DMA_TCD0_NBYTES_MLOFFNO
DMA_TCD0_NBYTES_MLOFFYES

 

Any help greatly appreciated.

0 Kudos
Reply
1 Solution
2,283 Views
konrada
Contributor IV

They refer to the same memory address, so it doesn't matter which one you use. Depending on the DMA settings, the TCDx_NBYTES field has a different bit layout, and the different names are one way of coping with that. (My guess is that Freescale uses a generator to generate header files and documentation from a chip description, and the generator doesn't support a register with varying bit layouts).

View solution in original post

0 Kudos
Reply
2 Replies
2,284 Views
konrada
Contributor IV

They refer to the same memory address, so it doesn't matter which one you use. Depending on the DMA settings, the TCDx_NBYTES field has a different bit layout, and the different names are one way of coping with that. (My guess is that Freescale uses a generator to generate header files and documentation from a chip description, and the generator doesn't support a register with varying bit layouts).

0 Kudos
Reply
2,283 Views
nijo
Contributor II
Thank you very much for you answer.
Just for future reference this is what I found after you "tip", this is taken from MK60N512VMD100.h

 

union {
uint32_t NBYTES_MLNO;
uint32_t NBYTES_MLOFFNO;
uint32_t NBYTES_MLOFFYES;
};

 

(That is, they do indead reference the exact same memory address).

0 Kudos
Reply