DMA peripheral request - KL25

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMA peripheral request - KL25

Jump to solution
4,392 Views
Fan_xy
Contributor III

Hello ,

As we know , kl25 has many dma peripheral requests and four DMA channels , and my question is when have a dma peripheral requests ,it will trigger which  DMA channle ?  where or which register config it  ?

Thank you!

0 Kudos
Reply
1 Solution
3,776 Views
mjbcswitzerland
Specialist V

Hi

You define which peripheral trigger is used for each DMA channel in the DMAMUX.

Registers are

DMAMUX0_CHCFG0

DMAMUX0_CHCFG1

DMAMUX0_CHCFG2

DMAMUX0_CHCFG3

Regards

Mark

View solution in original post

0 Kudos
Reply
6 Replies
3,776 Views
mjbcswitzerland
Specialist V

Hi

You define which peripheral trigger is used for each DMA channel in the DMAMUX.

Registers are

DMAMUX0_CHCFG0

DMAMUX0_CHCFG1

DMAMUX0_CHCFG2

DMAMUX0_CHCFG3

Regards

Mark

0 Kudos
Reply
3,776 Views
Fan_xy
Contributor III

hi Mark,

Thank you for help.

I find your said , use DMAUX0_CHCFGN -> SOURCE  define , while  where can find the peripheral trigger's slot number? for example , now i use UART _DMA trigger  DMA0 , the  slot number is ?  or the DMAMUX0_CHCFG0  is ?

Best Regards

Linda

0 Kudos
Reply
3,776 Views
mjbcswitzerland
Specialist V

Linda

These are the trigger defines that I use when working with the KL devices (not all triggers are available on particular devices)

Regards

Mark

  #define DMAMUX_CHCFG_SOURCE_DISABLED   0                       // 0x00                  
  #define DMAMUX_CHCFG_SOURCE_UART0_RX   2                       // 0x02 UART0 RX - DMAMUX_CHCFG_xx are available on DMA MUX 0 and on DMA MUX 1 (when available)
  #define DMAMUX_CHCFG_SOURCE_UART0_TX   3                       // 0x03 UART0 TX
  #define DMAMUX_CHCFG_SOURCE_UART1_RX   4                       // 0x04 UART1 RX
  #define DMAMUX_CHCFG_SOURCE_UART1_TX   5                       // 0x05 UART1 TX
  #define DMAMUX_CHCFG_SOURCE_UART2_RX   6                       // 0x06 UART2 RX
  #define DMAMUX_CHCFG_SOURCE_UART2_TX   7                       // 0x07 UART2 TX
  #define DMAMUX_CHCFG_SOURCE_UART3_RX   8                       // 0x08 UART3 RX
  #define DMAMUX_CHCFG_SOURCE_UART3_TX   9                       // 0x09 UART3 TX
  #define DMAMUX_CHCFG_SOURCE_UART4_RX   10                      // 0x0a UART4 RX
  #define DMAMUX_CHCFG_SOURCE_UART4_TX   11                      // 0x0b UART4 TX
  #define DMAMUX_CHCFG_SOURCE_UART5_RX   12                      // 0x0c UART5 RX
  #define DMAMUX_CHCFG_SOURCE_UART5_TX   13                      // 0x0d UART5 TX
  #define DMAMUX_CHCFG_SOURCE_I2S0_RX    14                      // 0x0e I2S0 RX
  #define DMAMUX_CHCFG_SOURCE_I2S0_TX    15                      // 0x0f I2S0 TX
  #define DMAMUX_CHCFG_SOURCE_SPI0_RX    16                      // 0x10 SPI0 RX
  #define DMAMUX_CHCFG_SOURCE_SPI0_TX    17                      // 0x11 SPI0 TX
  #define DMAMUX_CHCFG_SOURCE_SPI1_RX    18                      // 0x12 SPI1 RX
  #define DMAMUX_CHCFG_SOURCE_SPI1_TX    19                      // 0x13 SPI1 TX
  #define DMAMUX_CHCFG_SOURCE_SPI2_RX    20                      // 0x14 SPI2 RX
  #define DMAMUX_CHCFG_SOURCE_SPI2_TX    21                      // 0x15 SPI2 TX
  #define DMAMUX0_CHCFG_SOURCE_I2C0      22                      // 0x16 I2C0 - DMAMUX0_CHCFG_xx are only available on DMA MUX 0
  #define DMAMUX0_CHCFG_SOURCE_I2C1_2    23                      // 0x17 I2C1 (or I2C2)
  #define DMAMUX_CHCFG_SOURCE_FTM0_C0    24                      // 0x18 FTM0/TPM0 channel 0
  #define DMAMUX_CHCFG_SOURCE_FTM0_C1    25                      // 0x19 FTM0/TPM0 channel 1
  #define DMAMUX_CHCFG_SOURCE_FTM0_C2    26                      // 0x1a FTM0/TPM0 channel 2
  #define DMAMUX_CHCFG_SOURCE_FTM0_C3    27                      // 0x1b FTM0/TPM0 channel 3
  #define DMAMUX_CHCFG_SOURCE_FTM0_C4    28                      // 0x1c FTM0/TPM0 channel 4
  #define DMAMUX_CHCFG_SOURCE_FTM0_C5    29                      // 0x1d FTM0/TPM0 channel 5
  #define DMAMUX_CHCFG_SOURCE_FTM0_C6    30                      // 0x1e FTM0/TPM0 channel 6
  #define DMAMUX_CHCFG_SOURCE_FTM0_C7    31                      // 0x1f FTM0/TPM0 channel 7
  #define DMAMUX0_CHCFG_SOURCE_FTM1_C0   32                      // 0x20 FTM1/TPM1 channel 0
  #define DMAMUX0_CHCFG_SOURCE_FTM1_C1   33                      // 0x21 FTM1/TPM1 channel 1
  #define DMAMUX0_CHCFG_SOURCE_FTM2_C0   34                      // 0x22 FTM2/TPM2 channel 0
  #define DMAMUX0_CHCFG_SOURCE_FTM2_C1   35                      // 0x23 FTM2/TPM2 channel 1
  #define DMAMUX_CHCFG_SOURCE_IEEE1588_T036                      // 0x24 IEEE 1588 timer 0 (alternative)
  #define DMAMUX0_CHCFG_SOURCE_FTM3_C1   36                      // 0x24 FTM3 channel 1
  #define DMAMUX_CHCFG_SOURCE_IEEE1588_T137                      // 0x25 IEEE 1588 timer 1 (alternative)
  #define DMAMUX0_CHCFG_SOURCE_FTM3_C2   37                      // 0x25 FTM3 channel 2
  #define DMAMUX_CHCFG_SOURCE_IEEE1588_T238                      // 0x26 IEEE 1588 timer 2 (alternative)
  #define DMAMUX0_CHCFG_SOURCE_FTM3_C3   38                      // 0x26 FTM3 channel 3
  #define DMAMUX_CHCFG_SOURCE_IEEE1588_T339                      // 0x27 IEEE 1588 timer 3 (alternative)
  #define DMAMUX_CHCFG_SOURCE_ADC0       40                      // 0x28 ADC0
  #define DMAMUX_CHCFG_SOURCE_ADC1       41                      // 0x29 ADC1
  #define DMAMUX0_CHCFG_SOURCE_CMP0      42                      // 0x2a CMP0
  #define DMAMUX0_CHCFG_SOURCE_CMP1      43                      // 0x2b CMP1
  #define DMAMUX0_CHCFG_SOURCE_CMP2      44                      // 0x2c CMP2
  #define DMAMUX_CHCFG_SOURCE_DAC0       45                      // 0x2d DAC0
  #define DMAMUX_CHCFG_SOURCE_DAC1       46                      // 0x2e DAC1
  #define DMAMUX0_CHCFG_SOURCE_CMT       47                      // 0x2f CMT
  #define DMAMUX0_CHCFG_SOURCE_PDB       48                      // 0x30 PDB
  #define DMAMUX0_CHCFG_SOURCE_PORTA     49                      // 0x31 port A
  #define DMAMUX0_CHCFG_SOURCE_PORTB     50                      // 0x32 port B
  #define DMAMUX0_CHCFG_SOURCE_PORTC     51                      // 0x33 port C
  #define DMAMUX0_CHCFG_SOURCE_PORTD     52                      // 0x34 port D
  #define DMAMUX0_CHCFG_SOURCE_PORTE     53                      // 0x35 port E
  #define DMAMUX0_CHCFG_SOURCE_TPM0_OVERFLOW                      
54// 0x36 TPM0 overflow
  #define DMAMUX0_CHCFG_SOURCE_TPM1_OVERFLOW         
55// 0x37 TPM1 overflow
  #define DMAMUX0_CHCFG_SOURCE_TPM2_OVERFLOW    
56// 0x38 TPM2 overflow
  #define DMAMUX0_CHCFG_SOURCE_TSI                                             
57                      // 0x39 TSI
  #define DMAMUX_CHCFG_TRIG              0x40                    // DMA channel trigger enable
  #define DMAMUX_CHCFG_ENBL              0x80                    // DMA channel enable
3,776 Views
Fan_xy
Contributor III

Hi Mark,

Thank for your help.

And i have another question,  now I want use DMA transmit ADC result data.  I need collect two different signals use two  ADC channles  . And the in  kl25 , all of the adc channels  dma trigger are called ADC0,  my question is now I can't  use two DMA channals transmit two ADC data ,  do you have any good idea ?

Thank you !

Linda

0 Kudos
Reply
3,776 Views
mjbcswitzerland
Specialist V

Linda

The KL25 has one ADC controller. You can configure it for HW triggered mode so that it samples two channels automatically.

The results are available in ADC0_RA and ADC0_RB so it is possible to transfer these by configuring a DMA channel to copy two 16 bit words from ADC0_RA address on each trigger. The result is the two channels at the destination - if a buffer, the two channels will be stored Channel A, Channel B, Channel A, Channel B etc,

Or you can program two DMA channels with the same trigger and each one can copy either ADC0_RA or ADC0_RB to a buffer so that the channel data is not alternating.

Regards

Mark

0 Kudos
Reply
3,776 Views
likong
NXP Employee
NXP Employee

You can search "DMA request source" in RM, and you would find a table.