DMA and CACHE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,582件の閲覧回数
sean_dvorscak
Contributor III

I am using a KE18F MCU.

I am using DMA to transfer received UART data into a circular queue.  I use the DADDR of the DMA channel that handles these actions and a pointer of "read" data to determine if new data has been put into the queue.

I am concerned that when I read my data queue, I will read what is in cache, instead of the what's actually in my queue.  Since there is no DMA coherency with cache.

I am wondering if I would need to search the cache and invalidate any data that is from my data queue when it comes time to process the received data, since the data was moved into the queue by DMA?

0 件の賞賛
返信
1 解決策
2,547件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Sean,

In this case, you are right, you do not need to worry about the cache, because you are using the FlexRAM and it is not cacheable.

2. Non-cacheable — access to address spaces with this cache mode are not cacheable.
These accesses bypass the cache and access the output bus. In other words, it doesn't affect this process.

Regards,

Mario

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,566件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Sean,

I hope you are doing great.

You are passing the UART received from UART to a circular buffer. What do you mean cache in this case?

You only have to be sure that you read out the data from the circular buffer before the DMA writes again to that section.

Regards,

Mario

 

0 件の賞賛
返信
2,565件の閲覧回数
sean_dvorscak
Contributor III

I am referring to when I process what is in my queue.  The data is moved into the queue by DMA, but there is no cache hardware coherency.  So when my software comes to reading the queued data, I am concerned what I might read.  Will I read what is in cache, or in RAM?

I did read though in table 14-1 in the KE18F manual that RAM is non-cacheable.  Can you confirm if this means that I don't have worry about this?

sean_dvorscak_0-1604958266794.png

 

0 件の賞賛
返信
2,548件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Sean,

In this case, you are right, you do not need to worry about the cache, because you are using the FlexRAM and it is not cacheable.

2. Non-cacheable — access to address spaces with this cache mode are not cacheable.
These accesses bypass the cache and access the output bus. In other words, it doesn't affect this process.

Regards,

Mario

0 件の賞賛
返信