DMA - UART receive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMA - UART receive

1,866 Views
ksaiviswanadhul
Contributor II

Hi,

i am using kinetis k60 board. i'm facing issue on receiving multiple characters in dma uart receive please help me below attached code... i want to receive multiple bytes but i'm receiving single byte only.

 

void dma_receive(DMA_MemMapPtr dmach , uint8_t ch , uint8_t* val)
{
int j;
int i;
for(i=0;i<100;i++);


DMA_SADDR_REG(dmach , ch) =0;
//DMA_CR |= DMA_CR_EMLM_MASK;
DMA_SADDR_REG(dmach , ch)|= DMA_SADDR_SADDR(0x4006B007); // CONFIGURING SOURCE ADDRESS
for( j =0 ; j<1000; j++);

DMA_SOFF_REG(dmach,ch) =0;
DMA_TCD0_SLAST= 0x0;
DMA_ATTR_REG(dmach , ch) = (DMA_ATTR_SSIZE(0) | DMA_ATTR_DSIZE(0)); //CONFIGURING SOURCE ADDRESS SIZE


// DMA_NBYTES_MLOFFNO_REG(dmach , ch) = DMA_NBYTES_MLOFFNO_SMLOE_MASK|DMA_NBYTES_MLOFFNO_DMLOE_MASK| DMA_NBYTES_MLOFFNO_NBYTES(0x01);
//

DMA_NBYTES_MLNO_REG(dmach , ch) = 0;

DMA_NBYTES_MLNO_REG(dmach , ch)|= (DMA_NBYTES_MLNO_NBYTES(0x01));
DMA_DADDR_REG(dmach , ch) = 0;
DMA_DADDR_REG(dmach , ch) |= DMA_DADDR_DADDR(val); //CONFIGURING DESTINATION ADDRESS ADDRESS

DMA_DOFF_REG(dmach , ch) = DMA_DOFF_DOFF(0x01);


DMA_BITER_ELINKNO_REG(dmach , ch) =0;

DMA_BITER_ELINKNO_REG(dmach , ch) = DMA_BITER_ELINKNO_BITER(0x01); //STARTING MAJOR ITERATION COUNT
DMA_CITER_ELINKNO_REG(dmach , ch) =0;
DMA_CITER_ELINKNO_REG(dmach , ch) = DMA_CITER_ELINKNO_CITER(0x01); // CURRENT MAJOR ITERATION COUNT




DMA_SERQ |= DMA_SERQ_SERQ_MASK;

DMA_CSR_REG(dmach , ch) = DMA_CSR_START_MASK; // START THE DMA



}

0 Kudos
Reply
2 Replies

1,826 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello ksaiviswanadhul

 

I suggest you to refer into the SDK examples. There you can find an example that shows how to use the UART driver with eDMA.

 

Let me know if this is helpful, if you have more questions do not hesitate to ask me.

Best regards,

Omar

0 Kudos
Reply

1,760 Views
ksaiviswanadhul
Contributor II

There are four QT5 browsers available in imx8qmmek  . QtWebEngine browsers can be found in:

1). /user/share/qt5/examples/webenginewidgets/stylesheetbrowser

2). /user/share/qt5/examples/webenginewidgets/simplebrowser

3). /user/share/qt5/examples/webenginewidgets/cookiebrowser

4). /user/share/qt5/examples/webenginewidgets/quicknanobrowser.

 

could you please tell me difference between 4 types?

0 Kudos
Reply