DMA UART RECEIVE K60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMA UART RECEIVE K60

1,852 Views
mdrasool_yadwad
Contributor II

hello,

I am facing problems in receive. I want to receive 4 bytes and store in the buffer but the buffer is loaded with same value. below i have written my code please go through it .

 


//Receive Function

{
DMA_SADDR_REG(dmach , ch) =0;

DMA_SADDR_REG(dmach , ch)|= DMA_SADDR_SADDR(0x4006B007); // CONFIGURING SOURCE ADDRESS
DMA_SOFF_REG(dmach,ch) =0;

DMA_ATTR_REG(dmach , ch) = (DMA_ATTR_SSIZE(0) | DMA_ATTR_DSIZE(0)); //CONFIGURING SOURCE ADDRESS SIZE

DMA_NBYTES_MLNO_REG(dmach , ch) = 0;

DMA_NBYTES_MLNO_REG(dmach , ch)|= (DMA_NBYTES_MLNO_NBYTES(0x04));
DMA_DADDR_REG(dmach , ch) = 0;
DMA_DADDR_REG(dmach , ch) |= DMA_DADDR_DADDR(val); //CONFIGURING DESTINATION ADDRESS ADDRESS


DMA_DOFF_REG(dmach , ch) = DMA_DOFF_DOFF(0x01);


DMA_BITER_ELINKNO_REG(dmach , ch) =0;
DMA_BITER_ELINKNO_REG(dmach , ch) = DMA_BITER_ELINKNO_BITER(0x4); //STARTING MAJOR ITERATION COUNT
DMA_CITER_ELINKNO_REG(dmach , ch) =0;
DMA_CITER_ELINKNO_REG(dmach , ch) = DMA_CITER_ELINKNO_CITER(0x4); // CURRENT MAJOR ITERATION COUNT


DMA_SERQ |= DMA_SERQ_SERQ_MASK;

DMA_CSR_REG(dmach , ch) = DMA_CSR_START_MASK; // START THE DMA

}

Labels (1)
0 Kudos
Reply
2 Replies

1,842 Views
mjbcswitzerland
Specialist V

Hi

It looks like you are triggering the DMA using the software method which makes it copy the Rx data immediately and therefore it is is not transferring received data but instead just the value that happens to be in the buffer.

Have you set up the DMUX to trigger on Rx data?

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or product development requirements

 

0 Kudos
Reply

1,829 Views
mdrasool_yadwad
Contributor II

Yes I have DMUX to trigger on Rx data. But i am getting same data again and again. Don't know to do it i am really confused and struck in this.

0 Kudos
Reply