DMA Scatter/Gather loads wrong adress in TCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DMA Scatter/Gather loads wrong adress in TCD

1,575件の閲覧回数
AnEngineer
Contributor II

Hi together,

I have a problem implementing the scatter/gather mechnism for the eDMA. My Processor is a MK61FN1M0VMJ15.

When finished the major loop, the field DLAST_SGA is added to the current DADDR.

But because of the fact, that the E_SG Bit (Enable Scatter/Gather) is set, this address should NOT be added, but the new TCD should be copied from this adress.

I found an errata for such a case, but I am not sure, if it is for this processor. (4N86B, e4626)

Following the code:

volatile uint32_t TCD_SG[] = {

      (uint32_t)&testArray, 0x02020004,

      0x00000004, 0xFFFFFFEC,

      0x80000020, 0x00050004,

      0xFFFFFFEC, 0x00050001,

   };

static int32_t testArray[10] = { 1, 2, 3, 4, 5, 6, 7, 8, 9, 10};

void InitDMA(void)

{

#ifdef __arm__

 

   // DMA Request for rising edge; Port as GPIO;

   PORTB->PCR[2] &= ~PORT_PCR_IRQC_MASK &~PORT_PCR_MUX_MASK;

   PORTB->PCR[2] = PORT_PCR_IRQC(1) | PORT_PCR_MUX(1);

  

   // Enable clock for DMAMUX and DMA

    SIM->SCGC6 |= SIM_SCGC6_DMAMUX0_MASK;

    SIM->SCGC7 |= SIM_SCGC7_DMA_MASK;

           

    // Enable Channel 0 and set PORTF (FPGA_INT#2) as DMA request source

    DMAMUX0->CHCFG[0] |= DMAMUX_CHCFG_ENBL_MASK | DMAMUX_CHCFG_SOURCE(50);

  

    // Enable request signal for channel 0

    DMA0->ERQ |= DMA_ERQ_ERQ0_MASK;// | DMA_ERQ_ERQ1_MASK;

       

    // Set memory address for source and destination

    DMA0->TCD[0].SADDR = (uint32_t)&testArray;

    DMA0->TCD[0].DADDR = DDR_ADRESS_START;

    // Set an offset for source and destination address

    DMA0->TCD[0].SOFF = 0x04; // Source address offset per transaction

    DMA0->TCD[0].DOFF = 0x04; // Destination address offset per transaction

       

    // Set source and destination data transfer size 32bit

    DMA0->TCD[0].ATTR = DMA_ATTR_SSIZE(2) | DMA_ATTR_DSIZE(2);

       

    // Number of bytes to be transfered in each service request of the channel

    DMA0->TCD[0].NBYTES_MLNO = 0x04; // 4 Bytes pro Minor Loop

       

    // Current major iteration count (a single iteration of 5 bytes)

    DMA0->TCD[0].CITER_ELINKNO = DMA_CITER_ELINKNO_CITER(5);

    DMA0->TCD[0].BITER_ELINKNO = DMA_BITER_ELINKNO_BITER(5);

   

    // Adjustment value used to restore the source and destiny address to the initial value

    DMA0->TCD[0].SLAST = -0x14;           // Source address adjustment

    DMA0->TCD[0].DLAST_SGA = (uint32_t)&TCD_SG[0];    // Destination address adjustment

  

    // Setup control and status register

    DMA0->TCD[0].CSR = 0;

    DMA0->TCD[0].CSR |= DMA_CSR_ESG_MASK;

#else

#endif

}

K_MASK | DMA_CSR_MAJORLINKCH(1);

0 件の賞賛
返信
1 返信

1,213件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi

Please refer to this experiment doc to implement the scatter/gather function.

使用DMA降低SPI通信过程中内核负荷 Reduce core work load with DMA Module during SPI communication


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信