DMA Channel linking arbitration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DMA Channel linking arbitration

ソリューションへジャンプ
3,444件の閲覧回数
sean_dvorscak
Contributor III

I was wondering how DMA channel link requests are stored, and how they affect arbitration.

Just to give an example, lets say DMA Ch 0 links to DMA Ch 1 when Ch 0 completes its major loop.  The priority of the channels is set for higher channels having priority over lower channels.  If DMA Ch 2 sends a request while DMA Ch 0 is working, when Ch 0 finishes, will DMA service Ch 1 or Ch 2 next?  Does DMA finish all the channel links before servicing any other requests?

The reference manual makes it seem that the DMA channel linking is not considered a hardware request, so you cannot view the requests in the HRS register.  So how does DMA store the requests for linking?

0 件の賞賛
返信
1 解決策
3,394件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Sean,

Having preemption disabled will mean that channel transfers will not be suspended, therefore, DMA will attend the request that came first.

Best regards,

Felipe

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,421件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Sean,

In this case the linked channel will take place once the major loop is completed. So in the scenario you shared as Ch 0 is still working then preemption will occur and the lower priority channel will halt its transfer and allows the channel of higher priority to carry out its transfer. After the completion of major loop then linked channel will take place.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

0 件の賞賛
返信
3,417件の閲覧回数
sean_dvorscak
Contributor III

Hello Felipe,

I should have also mentioned that I have preemption disabled.

The scenario is more about what will happen if Ch 0 is supposed to link to Ch1, but there is already a DMA request for Ch 2 when Ch 0 finishes the major loop.  Will it finish the link chain first, or will it service Ch 2 after Ch 0?

0 件の賞賛
返信
3,395件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Sean,

Having preemption disabled will mean that channel transfers will not be suspended, therefore, DMA will attend the request that came first.

Best regards,

Felipe

0 件の賞賛
返信