DAC 6 bits MKM33

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DAC 6 bits MKM33

1,403件の閲覧回数
andresbaena
Contributor II

hello

i am disign a proyect, but i need a example code for DAC MKM33ZA128.

thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,253件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

The 6-bit DAC is the part of the CMP module, you can gain an insight into it after reviews the page 509 through the link as below.

http://cache.nxp.com/files/microcontrollers/doc/ref_manual/MKMxxZxxCxx5RM.pdf?fpsp=1&WT_TYPE=Referen...
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信