D4D_CONSOLE save text

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

D4D_CONSOLE save text

ソリューションへジャンプ
5,209件の閲覧回数
Thommi_Tulpe
Contributor IV

Hello,

is it possible to save the whole text of a console in an array ?

 

Can I set the cursor on the position  with a touch on the touchscreen?

 

Thanks

0 件の賞賛
返信
1 解決策
4,843件の閲覧回数
Thommi_Tulpe
Contributor IV

Thank you Luis, thank you Gargy

for your help.

 

I posted the cursor problem in another message.

 

Best Regards

Thomas

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
4,843件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

 

Console object has an internal text array:

static D4D_CHAR name##_txtArray[line_cnt][char_cnt + 1];\

 

You can copy that array (line by line) to different array.

 

You can detect the touch in cosole with pOnUsrMsg call back function defined. Then, if the message is D4D_MSG_TOUCHED, calculate the position of cursor with the touch position [

D4D_POINT D4D_GetTouchScreenCoordinates(void);]

 and move the cursor accordinly.

D4D_CnslGoToXY(D4D_OBJECT_PTR pObj, D4D_POINT newPosition)

 

I have never done, but I think is possible.

 

Bets Regards,

0 件の賞賛
返信
4,843件の閲覧回数
Thommi_Tulpe
Contributor IV

Hello,

and thank you for your fast answer.

 

Were is the name##_txtArray[line_cnt][char_cnt + 1] array defined and what do I have to write for

name## ?

My Console is declared as followd:

D4D_DECLARE_STD_CONSOLE(scrMain_Cons, "Kinetis Assembler", 0, 0, 320, 214, 100, 20,&bmpFreescale, FONT_ARIAL7, FONT_BERLIN_SANS_FBDEMI12)

 

Can I highlite the cursor by setting any flag ?

 

 

Thanks and have a nice weekend

 

 

0 件の賞賛
返信
4,843件の閲覧回数
Thommi_Tulpe
Contributor IV

Hello,

i found the text array. It is called scrMain_Cons_textArray[x][y].

But in this array I can't see the first line. The array beginns with the first character of the second line in [0][0].

 

Thanks

Thomas

0 件の賞賛
返信
4,843件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hi Thommi,

 

That is not the right array.

 

If you run the eGUI demo, you can add watch : scrLog_CnslLog_txtArray See attached image. You will see all the lines in the array. 'name' must be the name of the console object.

 

Regarding cursor,

D4D_CNSL_CURSOR_BLINK_TICK_COUNTER

is the constant to define the blink period, 0 is no cursor.

 

Best Regards,

0 件の賞賛
返信
4,843件の閲覧回数
Thommi_Tulpe
Contributor IV

Hello Luis,

thank you for your answer.

 

I think I have the right array. Im not using the demo.

I have a Console on the main screen (d4d_screen_main.c).

The Console is decleard as:  D4D_DECLARE_SCREEN_OBJECT(scrMain_Cons)

So the array has the name: scrMain_Cons_txtArray[ ][ ] .

And in this array I can´t see the firs line. The array begins with the caracters of the second line of the Console.

 

The  macro D4D_CNSL_CURSOR_BLINK_TICK_COUNTER is set to 10 (default) but the

cursor will not blink (I can't see the cursor)

Do I have to set a flag in the d4d_user_cfg.h file ?

 

Thank you

Thomas

 

 

0 件の賞賛
返信
4,843件の閲覧回数
Gargy
NXP Employee
NXP Employee

Hi,

 regarding to cursor, the issue should be that you have to also periodically call (in some function on time event) function void D4D_TimeTickPut(void) that notify eGUI about new time event and the macro D4D_CNSL_CURSOR_BLINK_TICK_COUNTER define how many these tick will be needed to blink with cursor.

 

And I take a look on the issue with array and let you now later in this thread.

 

Gargy

0 件の賞賛
返信
4,843件の閲覧回数
Gargy
NXP Employee
NXP Employee

Hi,

 regarding the first line in D4D_CONSOLE object:

The line is normally stored on end of defined text array (from any historical reason) but if want to move it on start of console array try to change this line in d4d_console.h :

static D4D_CNSL_DATA name##_data = { line_cnt - 1, {0, 0}, D4D_FALSE, 0, 0};\

to this state

static D4D_CNSL_DATA name##_data = { /*line_cnt - 1*/ 0, {0, 0}, D4D_FALSE, 0, 0};\

 

I try it and everithig looks fine but this is without any warranty :-D

 

Gargy

0 件の賞賛
返信
4,843件の閲覧回数
Thommi_Tulpe
Contributor IV

Hello Gargy,

thank you,t he cursor is blinking and the array is O.K.

 

I also have a little problem with the cursor.

When I put the cursor to a special position with

the command

cursor_position.x = 1;
cursor_position.y = 2;
(void) D4D_CnslGoToXY(&scrMain_Cons, cursor_position);

 

The cursor is displayed at the last position of the correct line.

 

After that I insert a character with the command:

(void)D4D_CnslPutString(&scrMain_Cons, "X");

The "X" is on position  1 in line 2, but the cursor is showen at the end of the line.

 

For your information, im writing code for a virtual keyboard.

 

Thank you

 

Thomas

 

 

0 件の賞賛
返信
4,844件の閲覧回数
Thommi_Tulpe
Contributor IV

Thank you Luis, thank you Gargy

for your help.

 

I posted the cursor problem in another message.

 

Best Regards

Thomas

0 件の賞賛
返信