Custom USB class

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Custom USB class

2,458件の閲覧回数
martindusek
Contributor V

Hi, I have SDK 2.3.1 for K22. There is no suitable USB class for my application (HID, CDC, ...) and I want to implement custom one. It will have bulk in, bulk out, interrupt in and interrupt out endpoint. Is there any document that describes how to implement custom usb class for the usb stack?

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,204件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Well for this issue, I would like recommend you may have a look at the Composite Device User's Guide, which can been found under: "~\KSDK_2.3\doc\usb, there are steps you may follow to build a custom composite demo.

0 件の賞賛
返信

2,204件の閲覧回数
dhanapal_rajend
Contributor II

I am using FRDMK82F, I need to configure the K82 as Bio-metric USB Device(custom class to support windows hello feature). Which USB class should I take as a reference? I am using SDK_2.3.1_MK82FN256xxx15 and MCUXpresso IDE v10.2.1 [Build 795] [2018-07-25].

Need your input for this implementation.

0 件の賞賛
返信