Custm trim reference Ke04 in debug mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Custm trim reference Ke04 in debug mode

1,363件の閲覧回数
IlConte
Contributor IV

I use a KE04Z8 processor with Codewarrior for MCU and PEMICRO Multilin Universal programmer.

I need a custm trim reference frequency at 34560 .

If i program directly with pemicro comamnd (CUSTOMTRIMREF 34560) all is OK.

But if i use the codewarrior debug mode dont't work.

I set the custom trim value

TrimKe04Debug.jpg

When run in address 0x3FE - 0x3FF there isn't the trim value and hence the clock is wrong !

TrimKe04DebugFF.jpg

 

Thanks all

0 件の賞賛
返信
1 返信

1,347件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Hope you are well.
Unfortunately, the SCTRIM value is not loaded if the device is in debug mode. To load correctly the value from the reserved flash location the device must not be in debug mode.

I apologize for the inconvenience this may cause you. If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 件の賞賛
返信