Creating a new project in Code Warrior for Kinetics EA uC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Creating a new project in Code Warrior for Kinetics EA uC

1,828 Views
kaslewis
Contributor III

I am trying to program a Kinetics EA uC using Code Warrior but I do not see EA listed as one of the uC options. When I installed CW I installled ALL the options so it should be here somewere, any help would be very much apprechated.

Kas

Labels (1)
0 Kudos
Reply
2 Replies

1,625 Views
BlackNight
NXP Employee
NXP Employee

Hi Kas,

Are you using MCU V10.6?

Do you mean these KEA devices?

pastedImage_0.png

Have you installed the updates (menu Help > Install New Software) from

http://freescale.com/lgfiles/updates/Eclipse/MCU10_6/com.freescale.mcu.updatesite

?

Erich

0 Kudos
Reply

1,625 Views
kaslewis
Contributor III

Hello Erich,

I am using 10.5 as that is what came with the TRK-KEA kit, I have updated the software with no luck. I am now downloading 10.6 and will see how that works.

Kas

0 Kudos
Reply