Copy flash from one chip to another using JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Copy flash from one chip to another using JTAG

Jump to solution
2,250 Views
marlonsmith
Contributor IV

Hi everyone,

I've written some code for the K20 chip, and I'm wondering if it's safe to use a JTAG programmer to copy that code from one chip to another.  Is there anything in memory that's perhaps read-only or reserved that could cause problems when dumping the entire memory from one K20 to another?

Thanks

Marlon

Tags (2)
0 Kudos
Reply
1 Solution
2,056 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Martin

This really depends the JTAG programmer. As normal, if programmer support this function, it should be safe.

Best Regards

Paul

View solution in original post

0 Kudos
Reply
1 Reply
2,057 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Martin

This really depends the JTAG programmer. As normal, if programmer support this function, it should be safe.

Best Regards

Paul

0 Kudos
Reply