Continious conversion for Kinetis K ADC using AN4590

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Continious conversion for Kinetis K ADC using AN4590

2,302件の閲覧回数
sohalpatel
Contributor II

Hi,

I am working on Kinetis (K10) for the last year, and the question is regarding the use of DMA for ADC as mentioned in AN4590. Can I use the ADC in continuous conversion mode and not use the PDB trigger source? My intention is to make the conversion as fast as possible.

Regards

Sohal

ラベル(1)
タグ(3)
2 返答(返信)

1,767件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Sohalpatel

PDB is just a trigger signal, ADC itself can run in continuous mode. So you can use ADC without PDB trigger.

Hope my reply can help you.

Best Regards

Paul

1,767件の閲覧回数
sohalpatel
Contributor II

Hello Zhe Tian,

I am glad you can give me some helpful ideas here. I wish to use both ADC with their differential inputs in a sequence, so i would like to have a trigger mechanism which could go and change the next ADC index. This is similar to the operation demonstrated in the Application Note.

Regards,

Sohal

0 件の賞賛
返信