Hello,
I have 4 KL05 in a board, Can I connect the SWD_CLK and RESET pins of the 4 mcus?
Best regards
Solved! Go to Solution.
Hi Javier Hernandez,
No, you can connect SWD_DIO and RESET together, but not the SWD_CLK, each chip should have the independent SWD_CLK, otherwise, you can't program it.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Better if is possible for common SWD_DIO and RESET because so I can reduce the BOM.
If possible, that would be ideal.
Hi Javier Hernandez,
No, you can connect SWD_DIO and RESET together, but not the SWD_CLK, each chip should have the independent SWD_CLK, otherwise, you can't program it.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank you
I have common RESET and SWD_DIO pins in the 10pos. pin socket. and the 4 pads in the center of the board are the 4 SWD_CLK, one for each mcu.
Best regards
You are welcome!
This design is OK to debug for each MCU.
Have a great day,
Kerry