Configuring PIT for 5-9 Mhz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuring PIT for 5-9 Mhz

1,462件の閲覧回数
arunagunasekara
Contributor I

Hi

     I am using k20 Tower kit and want to generate PWM signal using periodic interrupt timer.In the board am using, CPU is 100Mhz, bus clock of 50 Mhz and PIT of 50 Mhz.  Maximum of how much frequency can be generated using PIT and is it possible to generate up to 9 Mhz?I configure one portB pin as GPIO. The PIT triggers the DMA when PIT counter becomes 0 and  DMA toggles the GPIO output signal. DMA is requested at the rising edge. When using PIT, DMAMUX source can be always enabled? IF I use always enabled, Will it make any problem when i use other DMA channels for External memory transfer.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,280件の閲覧回数
apanecatl
Senior Contributor II

Hi

0 件の賞賛
返信