Configure Flash Security

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configure Flash Security

865 Views
giampietropompo
Contributor I

Hi All,

I'm working with the MK22FN1M0Axxx12, our solution is based on Bootloader + Custom Application.

Now, I should enable the Secure Mode and I'm able to enable it changing the definition of the Flash_Config ( defined into the file startup_*.c ) of the Bootloader.

We have many device in field so I should enable the secure mode by our application, I have done the same steps changing the file startup_*.c of the Application's project but it seems that it doesn't work. 

So I have a doubs, is it possible enabling the secure mode from the application?

Best regards,

Giampietro Pomponio

0 Kudos
Reply
0 Replies