Configure ADC for fixed conversion rate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configure ADC for fixed conversion rate

1,186件の閲覧回数
martindusek
Contributor V

Hi, what is the easiest way to configure KL25 ADC to output conversions at a fixed rate of 50 Hz? Is it possible to achieve this using only the ADC module or do I have to use timer module to trigger each conversion at the correct moment?

ラベル(2)
0 件の賞賛
返信
1 返信

1,053件の閲覧回数
mjbcswitzerland
Specialist V

Hello Martin

If you set the ADC in continuous conversion mode with highest accuracy, slowest ADC clock, maximum HW averaging and longest time added it will fire at about 650Hz.

Therefore, the method to use to get accurate 50Hz triggering is to use hardware trigger mode based on a PIT timer.

Regards

Mark

Kinetis: µTasker Kinetis support

KL25: µTasker Kinetis FRDM-KL25Z support  / µTasker Kinetis TWR-KL25Z48M support
ADC/DAC: http://www.utasker.com/docs/uTasker/uTaskerADC.pdf

For the complete "out-of-the-box" Kinetis experience and faster time to market