Compilation error for Freedom bootloader in KDS 3.2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compilation error for Freedom bootloader in KDS 3.2.0

2,417 Views
dhanapal_rajend
Contributor II

I have a FRDM-K82F: Freedom Development Platform for K82, K81. I am trying to compile freedom_bootloader in KDS 3.2.0 and I am getting error. Document has the procedure for IAR but i am using KDS. 

Document has below procedure

"Select C/C++ Compiler, and the preprocessor tab. Scroll down in the defined symbols. Note that all unused interfaces are disabled. This is done to save code size and remove un needed interfaces."

I am not seeing any respective setting in KDS. 

If I try to compile then i am getting linker error.

Any comments please.

Regards

R.Dhanapal

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

2,292 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi R.Dhanapal:

Just did a quick test on KBOOT with Frdm-k82, it can compile  successfully with KDS 3.2 on my side. I would suggest you download from MCU Bootloader|NXP  and try it again.

NXP_Kinetis_Bootloader_2_0_0\NXP_Kinetis_Bootloader_2_0_0\targets\MK82F25615\kds\freedom_bootloader

pastedImage_1.png

Regards

Daniel

0 Kudos
Reply

2,292 Views
dhanapal_rajend
Contributor II

Hi Daniel,

I have a document "Payment Solutions Secure boot Lab Guide 1_r0.2" it has

the procedure for IAR but i am using KDS 3.2.0version. By any chance i can

get the KDS based document. This would be helpful for me to proceed further

in a quick way.

Regards

R.Dhanapal

On Thu, 05 Jul 2018 03:30:17 +0000 (UTC), "danielchen@fsl"

0 Kudos
Reply

2,292 Views
dhanapal_rajend
Contributor II

Hi Daniel,

Thank you very much for your support. Fresh copy of source is getting compiled. Old copy of source which is in my PC has some problem.

Regards

R.Dhanapal

0 Kudos
Reply

2,292 Views
mjbcswitzerland
Specialist V


Hi

http://www.utasker.com/kinetis/FRDM-K82F.html

In case of complications, KBOOT (and other) solutions are available at the link that build with all IDEs (http://www.utasker.com/kinetis/compilers.html)

Regards

Mark

0 Kudos
Reply