Comparator Frequency detection mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Comparator Frequency detection mode

3,375 Views
jagadeeshsurnen
Contributor II

we are having issues with frequency measurement. we saw DAC disabled in the comments but in the defination structure we noticed that DACEN bit is SET which is enabled.can you help me out in setting comparator frequency detection.
/**************************************************************************/ /*!
* @brief Comparator Frequency Detection Setting:
* - filter disabled,
* - hysteresis 5mv,
* - sample, windowing and trigger modes disabled,
* - high speed mode,
* - non-inverting polarity,
* - unfiltered signal propagated to output (disabled),
* - comparator enabled,
* - CMP filter disabled when CR1[SE]=0,
* - IRQ and DMA disabled,
* - DAC disabled.
*****************************************************************************/
#define CMP_FREQ_DETECT_MODE_CONFIG_EN_DAC(dac) \
(tCMP){ \
/* CR0 */ SET(CMP_CR0_FILTER_CNT(0)) |SET(CMP_CR0_HYSTCTR(3)), \
/* CR1 */ CLR(CMP_CR1_SE_MASK) |CLR(CMP_CR1_WE_MASK)| \
CLR(CMP_CR1_TRIGM_MASK) |SET(CMP_CR1_PMODE_MASK)| \
CLR(CMP_CR1_INV_MASK) |CLR(CMP_CR1_COS_MASK)| \
CLR(CMP_CR1_OPE_MASK) |SET(CMP_CR1_EN_MASK), \
/* FPR */ SET(CMP_FPR_FILT_PER(0x00)), \
/* SCR */ CLR(CMP_SCR_DMAEN_MASK) |CLR(CMP_SCR_IER_MASK)| \
CLR(CMP_SCR_IEF_MASK), \
/* DACCR */ SET(CMP_DACCR_DACEN_MASK) |CLR(CMP_DACCR_VRSEL_MASK)| dac \
}

Regards,

jagadeesh

0 Kudos
Reply
5 Replies

3,099 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Would you please tell us where can I get that example code?
So that I can help you check the problem easier.

If you need the DAC output as one of Reference Input, then you should enable this bit.

DACEN.PNG

Best Regards

Robin

0 Kudos
Reply

3,099 Views
jagadeeshsurnen
Contributor II

Hi robin,

i took the reference from

https://www.nxp.com/webapp/Download?colCode=KMSWDRVAPIRM_SW .

Regards,

jagadeesh

0 Kudos
Reply

3,099 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

I didn't find CMP_FREQ_DETECT_MODE_CONFIG_EN_DAC in cmp_test example(C:\Freescale\KM128SWDRV_R4_1_6\build\iar_7_40\projects\cmp_test)

Only find Comparator Frequency Detection Setting in DRM143SW(Kinetis M One-phase power meter Design Reference Manual )
Have you refer that example?

Comparator Frequency Detection Setting.PNG

Phase Voltage Frequency Measurement.PNG

Best Regards

Robin

3,099 Views
jagadeeshsurnen
Contributor II

hi robin ,

thanks for your help, got the frequency measurement. there was a problem with V2REF.

BR,

jagadeesh

0 Kudos
Reply

3,099 Views
jagadeeshsurnen
Contributor II

hi robin,

yes, i have referred that example.

Best Regards,

jagadeesh

0 Kudos
Reply