Comparator Frequency detection mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Comparator Frequency detection mode

3,409件の閲覧回数
jagadeeshsurnen
Contributor II

we are having issues with frequency measurement. we saw DAC disabled in the comments but in the defination structure we noticed that DACEN bit is SET which is enabled.can you help me out in setting comparator frequency detection.
/**************************************************************************/ /*!
* @brief Comparator Frequency Detection Setting:
* - filter disabled,
* - hysteresis 5mv,
* - sample, windowing and trigger modes disabled,
* - high speed mode,
* - non-inverting polarity,
* - unfiltered signal propagated to output (disabled),
* - comparator enabled,
* - CMP filter disabled when CR1[SE]=0,
* - IRQ and DMA disabled,
* - DAC disabled.
*****************************************************************************/
#define CMP_FREQ_DETECT_MODE_CONFIG_EN_DAC(dac) \
(tCMP){ \
/* CR0 */ SET(CMP_CR0_FILTER_CNT(0)) |SET(CMP_CR0_HYSTCTR(3)), \
/* CR1 */ CLR(CMP_CR1_SE_MASK) |CLR(CMP_CR1_WE_MASK)| \
CLR(CMP_CR1_TRIGM_MASK) |SET(CMP_CR1_PMODE_MASK)| \
CLR(CMP_CR1_INV_MASK) |CLR(CMP_CR1_COS_MASK)| \
CLR(CMP_CR1_OPE_MASK) |SET(CMP_CR1_EN_MASK), \
/* FPR */ SET(CMP_FPR_FILT_PER(0x00)), \
/* SCR */ CLR(CMP_SCR_DMAEN_MASK) |CLR(CMP_SCR_IER_MASK)| \
CLR(CMP_SCR_IEF_MASK), \
/* DACCR */ SET(CMP_DACCR_DACEN_MASK) |CLR(CMP_DACCR_VRSEL_MASK)| dac \
}

Regards,

jagadeesh

0 件の賞賛
返信
5 返答(返信)

3,133件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Would you please tell us where can I get that example code?
So that I can help you check the problem easier.

If you need the DAC output as one of Reference Input, then you should enable this bit.

DACEN.PNG

Best Regards

Robin

0 件の賞賛
返信

3,133件の閲覧回数
jagadeeshsurnen
Contributor II

Hi robin,

i took the reference from

https://www.nxp.com/webapp/Download?colCode=KMSWDRVAPIRM_SW .

Regards,

jagadeesh

0 件の賞賛
返信

3,133件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

I didn't find CMP_FREQ_DETECT_MODE_CONFIG_EN_DAC in cmp_test example(C:\Freescale\KM128SWDRV_R4_1_6\build\iar_7_40\projects\cmp_test)

Only find Comparator Frequency Detection Setting in DRM143SW(Kinetis M One-phase power meter Design Reference Manual )
Have you refer that example?

Comparator Frequency Detection Setting.PNG

Phase Voltage Frequency Measurement.PNG

Best Regards

Robin

3,133件の閲覧回数
jagadeeshsurnen
Contributor II

hi robin ,

thanks for your help, got the frequency measurement. there was a problem with V2REF.

BR,

jagadeesh

0 件の賞賛
返信

3,133件の閲覧回数
jagadeeshsurnen
Contributor II

hi robin,

yes, i have referred that example.

Best Regards,

jagadeesh

0 件の賞賛
返信