Coding custom interrupt routine, in a Processor Expert application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Coding custom interrupt routine, in a Processor Expert application

2,752件の閲覧回数
lucaag
Contributor III

Hello,

Due to lack of program memory, I need to re-write SPI interrupt routines, to optimize code size.

Are there any article or AN, describing how to interact with PE Generated_Code without causing any issue?

I've seen PE creates its own vector table, in file vector.c, but I wouldn't like to modify it.

Thank you in advance

Luca

0 件の賞賛
返信
3 返答(返信)

2,617件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Luca,

you can disable code generation for each component, see Disable my Code Generation | MCU on Eclipse .

I hope this helps,

Erich

2,617件の閲覧回数
lucaag
Contributor III

Thank you Erich.

The article is useful.

So, I should first generate the code, than modify and than disable the code generation. Is it correct?

 

Luca

0 件の賞賛
返信

2,617件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Luca,

yes, that's correct.

Erich