CodeWarrior support for MK60X256VLQ100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior support for MK60X256VLQ100

ソリューションへジャンプ
1,980件の閲覧回数
WadeJones
Contributor I

I'm working on my first project using CodeWarrior and I have a question regarding support for the Kinetis MK60X256VLQ100, which is the LQFP144 package. When I create the project and select the MK60 family, I only see support for the BGA package when I try to use the Device Initialization tool. I know I must be missing a selection somewhere, but I can't see it. Thanks for any help anyone might be able to provide.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,872件の閲覧回数
apanecatl
Senior Contributor II

Once you create the project selecting the processor variant (MK60DX256 / MK60DX256Z) and the Device Initialization tool, go to the Target CPU tab, and click on Select CPU package, a small window will pop up showing you the available packages, select MK60DX256VLQ10 (144 LQFP) and you're right on track.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,873件の閲覧回数
apanecatl
Senior Contributor II

Once you create the project selecting the processor variant (MK60DX256 / MK60DX256Z) and the Device Initialization tool, go to the Target CPU tab, and click on Select CPU package, a small window will pop up showing you the available packages, select MK60DX256VLQ10 (144 LQFP) and you're right on track.

0 件の賞賛
返信
1,872件の閲覧回数
WadeJones
Contributor I

That worked. Thanks for the help.

0 件の賞賛
返信