Code for SPI (Serial peripheral interface) using PCA8561BHN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Code for SPI (Serial peripheral interface) using PCA8561BHN

1,600 次查看
longoal025
Contributor I

Hi,,

Can anyone please post the code for SPI (Serial peripheral interface) using PCA8561BHN

I tried doing display but not work...

please post the code for SPI


Thank you

0 项奖励
回复
1 回复

1,588 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi  longoal025,

   Unfortunately, we don't have the directly PCA8561BHN sample code for your reference, but it is not complicated.

   I don't know which kinetis you are using, you can us the SDK code SPI driver:

https://mcuxpresso.nxp.com/

then you need to refer to PCA8561BHN datasheet, send the related command is OK:

https://www.nxp.com/docs/en/data-sheet/PCA8561.pdf

  You also can search it from the website:

https://bbs.elecfans.com/jishu_949427_1_1.html

It can give you some inclues.

 

Wish it helps you!

If you still have questions about it, please kindly let me know!

Best Regards,

Kerry

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-----------------------------------------------------------------------------

0 项奖励
回复