Code for 1ms withTMR module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code for 1ms withTMR module

1,577 Views
yashkumar
Contributor III

I have to generate delay for my MICRO S32KXXX for 1 ms second.

I have gone through number of post, which are related to LPTMR module to generate delay for application .

I also followed up the LPTMR module in K60P144M micro and tried here to write the code for generation dealy for 1 ms.

I want to use OSC0ERCLK clock for LPTMR module, my crystal is of 8 MHz.

 

Thanks!

Labels (2)
0 Kudos
Reply
1 Reply

1,415 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Please check the same question from below thread:

https://community.nxp.com/thread/434930 


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply