Clocks Configuration problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clocks Configuration problem

4,039 Views
cerma
Contributor IV

Hi All,

 

I want to SDK2.0 instead of Processor Expert. I have used „Clocks Configuration“ for clock configuration (export it attachment) and replaced directory in my project (made in KDS3.2) with this export. Program ends in „CLOCK_SetExternalRefClkConfig(oscsel);“ at „while (!(MCG->S & MCG_S_OSCINIT0_MASK))“. I have tried to enable pins for EXTAL0 and XTAL0. Is there anyone who knows, where is mistake? Is there any manual for web configurator?
I am using KL16Z128 with external crystal 16MHz and KDS3.2 with SDK2.0.

 

Thanks.

Original Attachment has been moved to: MKL16Z128xxx4_pins_sources_2017-01-23_14_06.zip

Original Attachment has been moved to: MKL16Z128xxx4_clocks_sources_2017-01-23_12_39.zip

0 Kudos
Reply
6 Replies

3,544 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry for the late reply!

Please try to enable the OSCERCLK.

Clock Tool.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,544 Views
Cdn_aye
Senior Contributor I

I have posted on a similar problem with the TWR-60DN. We are getting a hard fault in the clock module. I think the code generated is bad. It was noticed by an NXP moderator and he asked for more information last week, but have heard nothing since. So maybe you do not have a problem with your clock. What does work is the "Hello World" project from the Freertos site, at least for the TWR-60DN. As a suggestion you could try loading and running that project and see if you still have a clock problem. You don't need to bother with more than putting a break point in the first statement in Main.c. If you get that far your clock is ok.

0 Kudos
Reply

3,541 Views
cerma
Contributor IV

Thank you for advice but I would rather use „Clocks Configuration“ instead. It allows me to set various clock modes in processor. Besides if NXP provides this tool, it should work. HW is fine and project with Processor expert works as well with external crystal. I want to use „Clocks Configuration“ for KL16Z128 with external crystal 16MHz in PEE mode. Does anybody knows how to make it work?

0 Kudos
Reply

3,544 Views
mjbcswitzerland
Specialist V

Hi

This code will configure the KL16 to run in PEE at 48Mz (24MHz bus/flash) for a 16MHz crystal.
I show the actual register value writes in brackets []:

MCG_C2 = (MCG_C2_RANGE_8M_32M | MCG_C2_GAIN_MODE | MCG_C2_EREFS | MCG_C2_LOCRE0); // [0xa4 for low gain mode or 0xac for high gain mode] select crystal oscillator and select a suitable range
MCG_C1 = (MCG_C1_CLKS_EXTERN_CLK | MCG_C1_FRDIV_512); // [0xa0] switch to external source (the FLL input clock is set to as close to its input range as possible, although this is not absolutely necessary if the FLL will not be used)
while ((MCG_S & MCG_S_OSCINIT) == 0) {} // loop until the crystal source has been selected
while ((MCG_S & MCG_S_IREFST) != 0) {} // loop until the FLL source is no longer the internal reference clock
while ((MCG_S & MCG_S_CLKST_MASK) != MCG_S_CLKST_EXTERN_CLK) {} // loop until the external reference clock source is valid
MCG_C5 = ((CLOCK_DIV - 1) | MCG_C5_PLLSTEN0); // [0x27] now move from state FEE to state PBE (or FBE) PLL remains enabled in normal stop modes
MCG_C6 = ((CLOCK_MUL - MCG_C6_VDIV0_LOWEST) | MCG_C6_PLLS); // [0x58] set the PLL multiplication factor
while ((MCG_S & MCG_S_PLLST) == 0) {} // loop until the PLLS clock source becomes valid
while ((MCG_S & MCG_S_LOCK) == 0) {} // loop until PLL locks
SIM_CLKDIV1 = (((SYSTEM_CLOCK_DIVIDE - 1) << 28) | ((BUS_CLOCK_DIVIDE - 1) << 16)); // [0x10010000] prepare bus clock divides
MCG_C1 = (MCG_C1_CLKS_PLL_FLL | MCG_C1_FRDIV_1024); // [0x28] finally move from PBE to PEE mode - switch to PLL clock
while ((MCG_S & MCG_S_CLKST_MASK) != MCG_S_CLKST_PLL) {} // loop until the PLL clock is selected

Note that the MCG_C2 value depends on whether the crystal circuit needs high or low gain (whether it has feedback resistor and loading capacitors).
If set incorrectly the crystal will not start oscillating and you will get stuck waiting for the crystal source to be selected.

Regards

Mark

KL16/KL26: http://www.utasker.com/kinetis/FRDM-KL26Z.html
MCG: http://www.utasker.com/kinetis/MCG.html

0 Kudos
Reply

3,544 Views
cerma
Contributor IV

Thanks Mark for advice and I will test it for sure. MCG description is very understandable and useful. But I still would like to learn how to use "Clocks Configuration" tool. If it is provided by NXP (Qualcom) then I would like to use it. It seems that work with it should be easy. That is why I do not understand why there is nobody who can say what I am doing wrong and give me some kind of manual how to use "Clocks Configuration".

0 Kudos
Reply

3,544 Views
mjbcswitzerland
Specialist V

Hi

For Kinetis development the clock configuration represents a few lines of code and so probably 0.0001% of any project (it will already exist in a decent library). I have set this up for more than 250 Kinetis parts and configurations and never though of needing a tool to help since it is more flexible to understand the simple basics and just do it exactly as one wants.

I would invest energy in completing work accurately and well than getting annoyed with the manufacturer. These tools are basically PR gags to get people hooked on their chips, so shouldn't be an issue for professional developers.

Regards

Mark

0 Kudos
Reply