Clock deviation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clock deviation

4,131件の閲覧回数
smathad
Contributor II

Hi NXP community,

I had a few questions regarding the clock deviation using the 48MIRC on the K24. 

Firstly, I understand the from the datasheet that the open loop deviation from 0 to 85 degress is 1%.

 

48MIRC deviation.PNG

Q1. Is it correct to assume that the clock will deviate around 1% (approx. +/- 480000 clocks) between 0 to 85 degrees? Is there some kind of temperature distribution chart for the deviation? 

Q2. How will this clock deviation trickle down to the other clocks, bus clock and flash clock? We want to calculate  effect of clock deviation of each peripheral i.e., SPI, I2C, ADC and UART and in turn compare it with the tolerance given in the datasheet for these peripherals.

Any input will be very much appreciated. 

Thank you

Sachin  

ラベル(1)
2 返答(返信)

4,070件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Sachin,

1. yes, clock will deviate around 1% (approx. +/- 480000 clocks) between 0 to 85 degrees. But there is no such a chart.

2. If you use IRC48 as system clock source, of course it will trickle down to whole system. The deviation is proportional.

Regards,

Jing

3,605件の閲覧回数
marktverskoy
Contributor I

Hi, anybody knows what is IRC48 sensitivity to the MCU rail voltage VCC? 

0 件の賞賛
返信