Clock deviation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Clock deviation

3,857 次查看
smathad
Contributor II

Hi NXP community,

I had a few questions regarding the clock deviation using the 48MIRC on the K24. 

Firstly, I understand the from the datasheet that the open loop deviation from 0 to 85 degress is 1%.

 

48MIRC deviation.PNG

Q1. Is it correct to assume that the clock will deviate around 1% (approx. +/- 480000 clocks) between 0 to 85 degrees? Is there some kind of temperature distribution chart for the deviation? 

Q2. How will this clock deviation trickle down to the other clocks, bus clock and flash clock? We want to calculate  effect of clock deviation of each peripheral i.e., SPI, I2C, ADC and UART and in turn compare it with the tolerance given in the datasheet for these peripherals.

Any input will be very much appreciated. 

Thank you

Sachin  

标签 (1)
2 回复数

3,796 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Sachin,

1. yes, clock will deviate around 1% (approx. +/- 480000 clocks) between 0 to 85 degrees. But there is no such a chart.

2. If you use IRC48 as system clock source, of course it will trickle down to whole system. The deviation is proportional.

Regards,

Jing

3,331 次查看
marktverskoy
Contributor I

Hi, anybody knows what is IRC48 sensitivity to the MCU rail voltage VCC? 

0 项奖励
回复