Clock Setting Problem in Processor Expert Code for MK22FN512xxx12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clock Setting Problem in Processor Expert Code for MK22FN512xxx12

ソリューションへジャンプ
2,207件の閲覧回数
brunopaillard
Contributor III

Hi

The code that processor Expert generates to manage the clocks (set a new clock) on the MK22FN512 does not seem to allow HSRUN mode, except when it is initially set in CPU_CLOCK_CONFIG_0

More specifically, I believe the function CPU_SetClockConfiguration () in CPU_Init.c has the following error:

-     At line 767, the line "  if ((CPU_ClockConfigDescriptors[ClockConfigurationID].PowerMode & CPU_CLOCK_HSRUN_ENABLE_MASK) != 0U) {"   uses ClockConfigurationID, instead of [the argument of the function] ModeID

At that point, ClockConfigurationID has not been initialized to ModeID yet. So it really represents the last clock configuration, NOT the one we want.

-     Moving line 827"  ClockConfigurationID = ModeID;  /* Store clock configuration identifier */"   up, to before line 767 above resolves the problem.

This does not create an immediate problem because it seems that the CPU runs remarkably well at 120 MHz in RUN mode...! At least at room temperatures

Bruno

0 件の賞賛
返信
1 解決策
2,034件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

I was testing the behavior you are reporting and found the same behavior. I think this is a bug on the Processor Expert code.

I already reported the issue to the development team.

Thank you for your interest in the Freescale products.


Hope this information can help you.

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,034件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

I was testing the behavior you are reporting and found the same behavior. I think this is a bug on the Processor Expert code.

I already reported the issue to the development team.

Thank you for your interest in the Freescale products.


Hope this information can help you.

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,034件の閲覧回数
brunopaillard
Contributor III

Thanks Adrian!

Bruno

0 件の賞賛
返信