Clarification on I2S transmitters for K22DX256

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clarification on I2S transmitters for K22DX256

3,212 Views
scottm
Senior Contributor II

I'm looking for clarification on the I2S/SAI configuration on the K22DX256, namely the number of I2S transmitter channels.

Page 124 of the reference manual says the device includes one I2S:

scottm_0-1690342017456.png

Page 194 shows two TXD lines:

 

scottm_2-1690342078040.png

Which of these is correct?

Thanks,

Scott

 

 

0 Kudos
Reply
5 Replies

3,186 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you said that the K22 has ONE SAI module, each SAI module has two transmitter pins I2S0_TXD0/TXD1 and two receiver pins I2S0_RXD0/RXD1.

In I2S mode, each transmitter pin can transfer two channels, so two transmitter pins can transmit 4 channels.

Hope it is helpful

BR

XiangJun Rong

 

0 Kudos
Reply

3,182 Views
scottm
Senior Contributor II

That seems to be at odds with what the manual says, though:

scottm_0-1690401855106.png

 

scottm_1-1690401888520.png

 

scottm_2-1690401957415.png

If the K22DX256 does indeed have a second transmit line that would be wonderful news because I could use it for a project I thought it wouldn't be suitable for. I just don't see any indication that the second TX line exists aside from the entry in the pinout table. The debugger only shows one "I2S0_TDR", and MK22D6.h only lists I2S0_TDR0.

Thanks,

Scott

0 Kudos
Reply

3,154 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I am sorry, the SAI module of  K22DX256 just has one transmitter pin I2S0_TXD0 and one receiver pin I2S0_RXD0.

Pls refer to section 3.9.5.1 Instantiation information in K22P48M50SF4RM.pdf, which is RM of MK22DX128VLF5, MK22DX256VLF5.

The SAI transmitter/receiver pins are dependent part number for the same K22 family, some has 1 pin for each transmitter and receiver, some has 2 pins for each transmitter and receiver.

BR

XiangJun Rong

 

xiangjun_rong_0-1690423248618.png

 

0 Kudos
Reply

3,123 Views
scottm
Senior Contributor II

So the pinout information is wrong, correct? I couldn't find any newer revisions or documentation errata.

Scott

0 Kudos
Reply

3,114 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the pin out information is wrong for K22DX256

Only pin 34 can function as I2S0_TXD0, pin 33 can not function as I2S0_TDX1.

xiangjun_rong_0-1690535021794.png

Hope it is helpful

BR

XiangJun Rong

 

0 Kudos
Reply