Choose a development control motor kit for 3-phase BLDC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Choose a development control motor kit for 3-phase BLDC

1,355件の閲覧回数
dariodetomaso
Contributor I

Hi "Community" ,

i'm a newbie with Freescale's products.

I'm trying to understand if there is a " development control motor kit " for a 3-phase brushless DC motor.

My goal is to use a development control motor kit for a high power eletric motor.

This motor can support input voltage of 40V and input current of 25 A.

Do Your kit include the inverter stage?

Is there a development kit "suitable" for my motor?


Thanks in advance

Best regards.

D.Detomaso


ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,258件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, D Detomaso

Sorry, our demo platform cannot support such large current motor. But our application note might help you. You can find it from link http://cache.freescale.com/files/32bit/doc/app_note/AN4862.pdf?fasp=1&WT_TYPE=Application%20Notes&WT...

Hope my reply can help you.

Best Regards

Paul

0 件の賞賛
返信