Checking SPI Transmit and receive in KEA-128 using TRK-KEA128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Checking SPI Transmit and receive in KEA-128 using TRK-KEA128

2,398 次查看
vigneshbalaji
Senior Contributor I

Hi,

    I am checking SPI Transmit and receive using 2 KEA-128 Development Board.I am using one TRK-KEA128 board for transmit and another TRK-KEA-128 Board for receive. I am not able to get it right. I have attached the code for both SPI Transmit and receive Below.

 

I am using Port E for both connections are

 

Master   Slave

PTE0 -> PTE0 (SPI_SCK -> SPI_SCK)

PTE1 -> PTE2 (MOSI -> MISO)

PTE3 -> PTE3 (SS -> SS)

I have made only these connections, is it enough or do i need to do more connections?

I am not able to receive any data.I am seeing it on debug mode in spi_d global variable for the receive code to validate this.

 

Can you tell me what things I have to change to make SPI Transmit and receive work??? 

Original Attachment has been moved to: SPI_Master_Transmit.zip

Original Attachment has been moved to: SPI_slave_KEA_128.zip

标记 (3)
3 回复数

1,605 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi VIGNESH BALAJI,

1. About the sample code

 Please refer to your another post, I already give you the SPI sample code:

SPI slave KEA-128 

Please refer to the official code, and check your own code.

2. SPI connection

  Your connection is wrong.

Master   slave

MISO     MISO

MOSI     MOSI

SS        SS

CLK     CLK

pastedImage_3.png

You can't connect the MOSI in master to slave MISO,  you should connect MOSI in master to the MOSI in slave.

This is very important.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,605 次查看
vigneshbalaji
Senior Contributor I

Hi Kerry,

              I understood the connections, what I wanted to know here is Whether the code that I have attached for SPI_Transmit and SPI_receive are they right????

Can you cross check them and say me ????

0 项奖励
回复

1,605 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi VIGNESH BALAJI,

    Your code have some errors.

Master:

1.  select the SSEL as the SPI select pin instead of just GPIO.

   SPI0_C1 |= SPI_C1_SSOE_MASK;    
   SPI0_C2 |= SPI_C2_MODFEN_MASK; 

2. enable the PTE0, PTE1,PTE2,PTE3 pull up for working stable.

PORT_PUE1 |= PORT_PUE1_PTEPE0_MASK | PORT_PUE1_PTEPE1_MASK|PORT_PUE1_PTEPE2_MASK|PORT_PUE1_PTEPE3_MASK;

3. After enter main file, add a small delay for the power on stable.

int main(void){    
unsigned int i,j;
    Clk_Init();
    SPI_init();
    
    for(i=0;i<100;i++) for(j=0;j<65535;j++); // delay, wait for the system stable
    
    for(;;) {       
        SPI_write(0x21);
        uint8_t spi_d = SPI_read();
    }
    
    return 0;
}

Slave:

1.  select the SSEL as the SPI select pin instead of just GPIO.

   SPI0_C1 &= ~SPI_C1_SSOE_MASK;
   SPI0_C2 |= SPI_C2_MODFEN_MASK;

2. enable the PTE0, PTE1,PTE2,PTE3 pull up for working stable.

PORT_PUE1 |= PORT_PUE1_PTEPE0_MASK | PORT_PUE1_PTEPE1_MASK|PORT_PUE1_PTEPE2_MASK|PORT_PUE1_PTEPE3_MASK;

Then after connect two KEA128 together, it will work fine.

I have test your code on my TRK KEA128 board, it works ok.

pastedImage_6.png

Slave debug result:

pastedImage_7.png

Slave can receive the correct data 0x21 from master.

Logic analyzer wave:

pastedImage_8.png

I also attached my modified project for your reference.

Wish it helps you!

Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复