Changes required for converting from RMII to MII

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Changes required for converting from RMII to MII

1,961 Views
Mohsin455
Contributor IV

Hi All,

 

              I am using TWRK60N512 and MQX 3.8. I am using KSZ8895MQ with MII Interface on my custom board. I know there are issues, such that TWRK60N512 cannot be used in MII mode (as some of the pins are use for JTAG)  but I will be trying this on custom board.

 

I want to know what are the changes required in the MQX code for TWRK60N512 in order to convert from RMII to MII Interface.

 

Thanks,

Mohsin

 

 

 

 

0 Kudos
Reply
2 Replies

1,489 Views
egoodii
Senior Contributor III

The one obvious change in ...\MQX_RTOS\mqx\source\bsp\twrk60n512\init_enet.c structure:

const ENET_PARAM_STRUCT ENET_default_params[BSP_ENET_DEVICE_COUNT] = {

{

    &ENET_0,

    Auto_Negotiate,

    ENET_OPTION_RMII | ENET_OPTION_PTP_MASTER_CLK,

    BSPCFG_TX_RING_LEN, // # tx ring entries

    BSPCFG_TX_RING_LEN, // # large tx packets

    ENET_FRAMESIZE, // tx packet size

    BSPCFG_RX_RING_LEN, // # rx ring entries

    BSPCFG_RX_RING_LEN, // # normal rx packets - must be >= rx ring entries

    ENET_FRAMESIZE, // ENET_FRAMESIZE, // rx packet size

    BSPCFG_RX_RING_LEN, // # rx PCBs - should be >= large rx packets.

    0,

    0

    }

};

is to remove ENET_OPTION_RMII.

Yes, at a hardware level you will lose your JTAG 'trace' function (so of course mux them to ENET, such as in init_gpio.c).

Changes to the phy interface routines in ...\MQX_RTOS\mqx\source\io\enet\phy\phy_xxx are another matter.  Maybe you will luck out and your PHY will work with the 'common subset'.

 

--ERGII

0 Kudos
Reply

1,489 Views
Mohsin455
Contributor IV

Hi ERGII,

 

                  Thanks for your reply. What do you mean by " at a hardware level you will lose your JTAG 'trace' function (so of course mux them to ENET, such as in init_gpio.c)"

 

Thanks,

Mohsin

0 Kudos
Reply