Cannot program with CMSIS-DAP and MCUXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot program with CMSIS-DAP and MCUXpresso

1,645 Views
LArmstrong1985
Contributor III

Hi,

I've a strange problem with GUI FlashTool in MCUXpresso 11.2.1.

If I try to program my board with DapLink (CMSIS-DAP) when I click to Run... it do nothing

and I'm not getting any errors. All works well instead when I use it in debug.

The problem is also present in other PCs with the coupled MCUXpresso 11.2 and Windows 10 20H2 while on another PC with MCUXpresso 11.1.0 and Windows 10 1909 all works fine.

I tried to downgrade MCUXpresso and Windows 10 in this PC but I was unable to resolve.

Does anyone else have the same problem? Are you aware of compatibility problems with some versions of Windows or Mcuxpresso?

Thank you id advance

0 Kudos
Reply
1 Reply

1,633 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi fabiobenevento,

Can you use CMSIS-DAP to debug? If it can't debug too, maybe you can try to reinstall the driver. 

MCUXpresso IDE has updated to v11.3. If v11.2 can't work, you can update it.

 

Regards,

Jing

0 Kudos
Reply