Can the device with Hybrid BLE Thread Router Wireless Uart still control the LED on the board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can the device with Hybrid BLE Thread Router Wireless Uart still control the LED on the board?

1,335件の閲覧回数
sanjiv_gounder
Contributor I

I have flashed a board with Hybrid BLE Thread Router Wireless Uart and using NXP Toolbox it is successfully controlling the 3 other boards which are flashed with Router Enabled thread device. However when testing with LED and changing color or on and off led via coap CON POST the LED on the Ble+thread hybrid board does not work. The other boards work fine just the BLE board LED doesn't function. 

Is the device with BLE+thread Stack only act as a gateway or can I still control the LED on that board as well via the Toolbox app?

ラベル(1)
0 件の賞賛
返信
1 返信

1,235件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

If you try to change the LED State from the application it will not change the state if it's the same board, the loop back it's not supported. 


You could send the direction to another board and then redirect it to the board you are looking for with an special code or coap resource. 

Sorry for the inconvenience this might cause you. 

Regards, 

Estephania 

0 件の賞賛
返信