Can´t receive more than one byte by UART.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can´t receive more than one byte by UART.

ソリューションへジャンプ
5,315件の閲覧回数
patricio
Contributor IV

Hello all,

I am working with the FRDM-KL25Z and CodeWarrior 10.5. I am trying to send and receive several bytes by the UART, but I am not able to do so.

I am already able to receive one byte, but there is no way to receive more than one byte. Please let me show you what I am doing:

- I am using a terminal called Docklight to send 10 bytes through RS232. I designed a pcb with a 232 tranceciver, so the FRDM-KL25Z UART pins receive the proper voltage leveIs.

- I check by an oscilloscope that these 10 bytes arrive to the FRDM-KL25Z UART pins.

- Both the terminal and the FRDM-KL25Z are configured with 9600 bauds, 8 data bits, 1 stop bit and no parity.

- I use the AsynchroSerial component. Please find attached its settings.

I try to receive the datas by polling, so first I use the method GetCharsInRxBuf() in order to know the number of bytes I receive. And then, I try to charge all these bytes with the method RecvChar into an array. Please find attached the code in a screen capture.

The point is that GetCharsInRxBuf always tells that I receive only 1 byte.

Any clue what I am doing wrong? Thank you in advance.

0 件の賞賛
返信
1 解決策
4,946件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Aitor,

In the file UART.h under the Generated_Code folder you will find a macro called UART_INP_BUF_SIZE which is used in the file UART.c. This macro is the bytes that the peripheral is expecting so you can convert that macro into a variable and change that variable in every OnFullRxBuf function.

Please let me know if this information is useful or if I can do anything else for you.

Best regards,

Earl.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,946件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Aitor,

Why don't you use the function ASerialLdd1_ReceiveBlock? I think that it fits better with your application. In fact, the function UART_RecvChar uses the function ASerialLdd1_ReceiveBlock.

Also, the component Serial_LDD can be useful for you. I recommend you to take a look into it. It also includes a function to send or receive a block of data. This component is has a lower level of abstraction so is more efficient.

Best regards,

Earl.

0 件の賞賛
返信
4,946件の閲覧回数
patricio
Contributor IV

Thank you Earl,

I will have a look to your recommendations and see if I get something.

However, I still don’t understand what I was doing wrong.

BR.

Aitor Aranzabal

De: EarlOrlando

Enviado el: jueves, 23 de julio de 2015 22:22

Para: AITOR ARANZABAL

Asunto: Re: - Can´t receive more than one byte by UART.

<http://jiveon.jivesoftware.com/mpss/c/zwA/PDcDAA/t.1oy/vsj1S9XrS2SqJTesJSaEtw/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D> Freescale Community

Can´t receive more than one byte by UART.

reply from Earl <http://jiveon.jivesoftware.com/mpss/c/zwA/PDcDAA/t.1oy/vsj1S9XrS2SqJTesJSaEtw/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bSFptD52UNhkZRd210-2FIwQWXO21D1d1BJXlhaAsM4UJCEzuXqJS9olAmWqS5vTZ-2BAY-3D> Orlando Ramirez Sanchez in Kinetis Microcontrollers - View <http://jiveon.jivesoftware.com/mpss/c/zwA/PDcDAA/t.1oy/vsj1S9XrS2SqJTesJSaEtw/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bSWu-2FQYmmII2lvY0tnf-2BikHrJzZIRuMazuccgcUMGO7F-2BO2jA26dDrVQB9krc5ou8g-3D> the full discussion

0 件の賞賛
返信
4,946件の閲覧回数
patricio
Contributor IV

Hello again,

After playing arround with different possiblities, I was able to receive the 10 bytes. I discarded the polling and I worked with the event OnFullRxBuf(void).

I had to change the "Input buffer size" to 10 in the processor expert component features. Please have a look below. Please remind that I am using AsynchroSerial component.

pastedImage_0.png

In my application, I will know the number of bytes that I will receive each time, but not always will be 10 bytes. So I would need to change the input buffer size each time. Is it a way to do it by firmware? I mean inserting code. I am having a look in the datasheet of the "KL25 Sub-Family Reference Manual" in order to find the proper register, but no way

Thank you in advance.

0 件の賞賛
返信
4,947件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Aitor,

In the file UART.h under the Generated_Code folder you will find a macro called UART_INP_BUF_SIZE which is used in the file UART.c. This macro is the bytes that the peripheral is expecting so you can convert that macro into a variable and change that variable in every OnFullRxBuf function.

Please let me know if this information is useful or if I can do anything else for you.

Best regards,

Earl.

0 件の賞賛
返信
4,946件の閲覧回数
patricio
Contributor IV

Hello Earl,

I did it and it works. Great.

I had to protect the component from the overwritting in the processor expert generating code.

Thanks a lot.

0 件の賞賛
返信