Can't receive data on EP0 in control transfer for HID class

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can't receive data on EP0 in control transfer for HID class

跳至解决方案
1,775 次查看
chuckh
Contributor III

Hello,

My application is supposed to receive a 64 byte packet on EP0 in the form of a SET REPORT.  There is code in usb_framework.c in  USB_Control_Service() for class requests with non-zero size that calls _usb_device_recv_data().  However, when this function is called, my data buffer is not updated.  I added code to call _usb_device_get_transfer_status() after _usb_device_recv_data() and find that this function returns USB_STATUS_TRANSFER_IN_PROGRESS indefinitely.

Am I missing a call to another function to service the USB or perhaps there is something else I am missing?

Any help will be greatly appreciated.

标记 (6)
0 项奖励
回复
1 解答
1,378 次查看
chuckh
Contributor III

I figured out that the LONG_RECEIVE_TRANSACTION and LONG_SEND_TRANSACTION defines were messing me up.  Once I changed the Max Packet to 64 and removed these defines, it seems to be working fine.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,378 次查看
chuckh
Contributor III

It seems like the _usb_device_recv_data() sets up for the next receive, which I expect to be EP0 OUT transaction (Host to my device).  The USB sniffer shows this packet is acked, so where does it go in the stack?  Since it is on EP0, shouldn't I see this in the USB_Control_Service() function?

0 项奖励
回复
1,379 次查看
chuckh
Contributor III

I figured out that the LONG_RECEIVE_TRANSACTION and LONG_SEND_TRANSACTION defines were messing me up.  Once I changed the Max Packet to 64 and removed these defines, it seems to be working fine.

0 项奖励
回复