Can't get any USB Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't get any USB Interrupt

ソリューションへジャンプ
2,010件の閲覧回数
georgschmidt
Contributor III

Hi,

I'm trying to get the USB_FS-Module running in Device-Mode on the TWR-K60F120M System.

During initialisation I activate the USB-Reset Interrupt, the global USB-Interrupt in the NVIC and assign an ISR.

Then I apply a reset to the USB-Module by setting the USBRESET-Bit in the USBTRC0-Register.

But I don't get any Interrupt neither after powering up the tower nor after applying an USB-Connector to the TWR-SER-Module.

What do I do wrong?

Thanks for help,

Georg

0 件の賞賛
返信
1 解決策
1,891件の閲覧回数
georgschmidt
Contributor III

I have found my mistake.

I didn't use the proper clock settings in the SIM.

Nevertheless, thanks for reading!

Georg

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,892件の閲覧回数
georgschmidt
Contributor III

I have found my mistake.

I didn't use the proper clock settings in the SIM.

Nevertheless, thanks for reading!

Georg

0 件の賞賛
返信
1,891件の閲覧回数
Monica
Senior Contributor III

Sorry for the late reply, Georg, but it's great that you found and corrected the flaw...keep it going! :smileywink:

We'll be around!

Regards.

0 件の賞賛
返信