Can not program or erase km35z75m board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not program or erase km35z75m board

1,555 Views
shivangi_23
Contributor I

I have program Km35 Board by McuExpresso IDE using jlink connected to k20 JTAG port. After that, I was unable to view the opensda drive or the com port.

shivangi_23_1-1670680350037.png

shivangi_23_9-1670681064690.png

 

 

1. I've tried with Jlink Commander. JTAG is linked to j24 port on the km35 board, And program Board Using SWD For the first time I am Successful to program code but when I tried Second time I can not able program .

 

shivangi_23_4-1670680619958.png

download.png

 

 

 

 

 

 

 

 

 

 

 

I tried to plug in the USB and remove the J6 jumper to directly power mcu  and when I send connect command  I immediately put jumper back but still could not able to connect.

I connected JTAG to k20 JTAG port and download Bin for opensda I have Successfully load file but could not recover drive and after that when I  try connect Can not able to connect.

I have also change board but in other board also Facing the same issue.

How to restore Drive Back I need to programmed the board with the cmsis dap linkserver.

 

I have also attached video link pls check.

https://glidemtech-my.sharepoint.com/:v:/p/rushinm/EcjDymPle9hDjTGEflZW6okBKI43WYR4CXxd1JvUytNcMA

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,522 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @shivangi_23 

Could you please tell me the programs you are uploading to the board? Also, have you tried using another computer? Sometimes there are issues between versions of MCUXpresso and windows, could you provide me the versions too please.

I'll be waiting for your response,

Best Regards, Miguel.

0 Kudos
Reply