Can i use ulink pro jtag debugger with kinetis design studio or codewarrior ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can i use ulink pro jtag debugger with kinetis design studio or codewarrior ?

1,387件の閲覧回数
sameerarvikar
Contributor III

I have got ulinkpro debugger from armkeil ,can i use it with codewarrior for MCU or Kinetis design studio for debugging

0 件の賞賛
返信
2 返答(返信)

1,189件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello sameer,

I'm confirmed with ARM support,  the ULINK adapter are supported by ust uVision,

doesn't support KDS or CW.

And the support devices listed at the below site :

MDK5 Device List 

Hope it helps

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,189件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Sameer,

 You said KDS, so do you want to develop Kinetis chips ?

  I checked the ULINKpro seems doesn't support kinetis :

pastedImage_1.png

maybe I missed something , as to I know little about the ULINKpro, I can  ask the ARM support

for it if your need . And also you can test a simple project on your side .


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信