Can i use ulink pro jtag debugger with kinetis design studio or codewarrior ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can i use ulink pro jtag debugger with kinetis design studio or codewarrior ?

1,390 次查看
sameerarvikar
Contributor III

I have got ulinkpro debugger from armkeil ,can i use it with codewarrior for MCU or Kinetis design studio for debugging

0 项奖励
回复
2 回复数

1,192 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello sameer,

I'm confirmed with ARM support,  the ULINK adapter are supported by ust uVision,

doesn't support KDS or CW.

And the support devices listed at the below site :

MDK5 Device List 

Hope it helps

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,192 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Sameer,

 You said KDS, so do you want to develop Kinetis chips ?

  I checked the ULINKpro seems doesn't support kinetis :

pastedImage_1.png

maybe I missed something , as to I know little about the ULINKpro, I can  ask the ARM support

for it if your need . And also you can test a simple project on your side .


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复