Can community arrange a seperate folder for USB discussions?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can community arrange a seperate folder for USB discussions?

1,818 Views
kai_liu
Senior Contributor I

I found there are many discussions for USB stack. However these threads are all under Microcontrollers.

Can Freescale community make a seperate folder for USB stack, so we can focus on USB, rather than hardware platform.

Tags (1)
0 Kudos
Reply
3 Replies

1,653 Views
Monica
Senior Contributor III

Hello Kai,

It is an interesting proposal you make. I totally agree with you, there are many questions regarding USB stack. As for now, we could create a category called "USB" within the Kinetis space since we have tons of USB-related questions but not only for Kinetis platform.

Please let me know if this would help and we'll be happy to create that for you.

That would involve, of course, moving all content in there :smileywink:

Best regards,

Monica.

0 Kudos
Reply

1,653 Views
kai_liu
Senior Contributor I

Hello, Monica,

Yes, please.

I found some FAEs are following questions. If they are product oriented, putting USB questions under architects can be solved eventually. If there is not USB oriented FAE, then putting USB related questions into a seperate category may put them in an orphan category.

PS, you don't have to move ALL content by now, That is an extra work. I think some solved questions can be moved as a starting point, the community members can submit questions under that category by themselves later.

Thanks anyway.

0 Kudos
Reply

1,653 Views
Monica
Senior Contributor III

Hello Kai,

As you well say, some FAEs and TICS are following questions, but they are experts at other bunch of stuff, too. The magic with categories is they would not be orphans because they would still belong to Kinetis space, but they'd be much more organized.

That will be arranged soon.

Regards,

Monica.

0 Kudos
Reply