Can anyone suggest reset circuit interface or document related to it for KL16 family and K64 family?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can anyone suggest reset circuit interface or document related to it for KL16 family and K64 family?

1,479 Views
chromeankit
Contributor I

Need reset circuit for KL16 and K64...do we need RC circuit for reset pin or it will work without it...confused

0 Kudos
Reply
1 Reply

1,356 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Ankit Kumar,

    Both KL16 and K64 Reset_b pin need to add external 4.7K to 10K pull up resistor, and 0.1uf capacitor to ground.

   

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply