Can MKE14F512VLL16 support Quad SPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can MKE14F512VLL16 support Quad SPI

5,674件の閲覧回数
prathamesh_h_patil
Contributor I

Can I interface Quad SPI to MKE14F512VLL16 controller as it support LPSPI and How we can interface it please explain in details.

ラベル(1)
0 件の賞賛
返信
9 返答(返信)

5,659件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @prathamesh_h_patil ,

Yes, LPSPI can support QUAD SPI flash. You can refer to this link

https://community.nxp.com/t5/i-MX-RT/LPSPI-how-to-set-for-QSPI-flash-device/m-p/1177734

Unfortunately, we don't have any example of the LPSPI interfacing an external flash.

 

Regards,

Jing

0 件の賞賛
返信

5,654件の閲覧回数
prathamesh_h_patil
Contributor I

Thanks For confirmation.

Can you please share its QPSI frequency?

and what it support Like Single Data Rate (SDR) or Double Data Rate  (DDR)?

0 件の賞賛
返信

5,646件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @prathamesh_h_patil ,

Please see table 56 in datasheet. Frequency of operation can be max to fperiph/2.The max fperiph is from SPLLDIV2. So, max frequency is 168/2/2=42Mhz.

LPSPI doesn't support DDR.

 

Regards,

Jing

 

0 件の賞賛
返信

5,643件の閲覧回数
prathamesh_h_patil
Contributor I

Thanks for information,

 

Q1. Could you please share Application note for Quad SPI for Flash memory?

Q2. Does MKE14F512VLL16 controller has restriction on particular make Quad Flash memory should use or it is free for any make quad flash?

Q3. Can MKE14F512VLL16 support SPI based Graphical LCD? if yes please share example.

 

 

タグ(1)
0 件の賞賛
返信

5,637件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @prathamesh_h_patil ,

A1. No, there isn't.

A2. I think it is free for any QSPI flash.

A3. Yes, it can. But there isn't example.

 

Regards,

0 件の賞賛
返信

5,570件の閲覧回数
prathamesh_h_patil
Contributor I

Dear NXP team,

 

As per the MKE14F512VLL16 datasheet supply voltage is 2.7V to 5.5V, so the question is if we use 3.3V as supply then is it okay for all operations, or else do we need to connect the 5V power supply.
 
Kindly check and suggest which supply is better for controller performance 3.3V or 5V?
0 件の賞賛
返信

5,552件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @prathamesh_h_patil ,

Either 3.3v or 5v is okey. You can freely determine VDD according to peripheral circuit. There is no difference in performance.

Regards,

Jing

0 件の賞賛
返信

5,541件の閲覧回数
prathamesh_h_patil
Contributor I

Dear NXP team,

If my supply of the controller is 3.3V then can I connect the 5V peripheral signal to controller and Vice versa?

Please confirm it.

 

Regards,

Prathamesh Patil

0 件の賞賛
返信

5,532件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @prathamesh_h_patil ,

No, you'd better don't design like that.

 

Regards,

Jing

0 件の賞賛
返信