Can MKE14F512VLL16 support Quad SPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can MKE14F512VLL16 support Quad SPI

5,519 次查看
prathamesh_h_patil
Contributor I

Can I interface Quad SPI to MKE14F512VLL16 controller as it support LPSPI and How we can interface it please explain in details.

标签 (1)
0 项奖励
回复
9 回复数

5,504 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @prathamesh_h_patil ,

Yes, LPSPI can support QUAD SPI flash. You can refer to this link

https://community.nxp.com/t5/i-MX-RT/LPSPI-how-to-set-for-QSPI-flash-device/m-p/1177734

Unfortunately, we don't have any example of the LPSPI interfacing an external flash.

 

Regards,

Jing

0 项奖励
回复

5,499 次查看
prathamesh_h_patil
Contributor I

Thanks For confirmation.

Can you please share its QPSI frequency?

and what it support Like Single Data Rate (SDR) or Double Data Rate  (DDR)?

0 项奖励
回复

5,491 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @prathamesh_h_patil ,

Please see table 56 in datasheet. Frequency of operation can be max to fperiph/2.The max fperiph is from SPLLDIV2. So, max frequency is 168/2/2=42Mhz.

LPSPI doesn't support DDR.

 

Regards,

Jing

 

0 项奖励
回复

5,488 次查看
prathamesh_h_patil
Contributor I

Thanks for information,

 

Q1. Could you please share Application note for Quad SPI for Flash memory?

Q2. Does MKE14F512VLL16 controller has restriction on particular make Quad Flash memory should use or it is free for any make quad flash?

Q3. Can MKE14F512VLL16 support SPI based Graphical LCD? if yes please share example.

 

 

标记 (1)
0 项奖励
回复

5,482 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @prathamesh_h_patil ,

A1. No, there isn't.

A2. I think it is free for any QSPI flash.

A3. Yes, it can. But there isn't example.

 

Regards,

0 项奖励
回复

5,415 次查看
prathamesh_h_patil
Contributor I

Dear NXP team,

 

As per the MKE14F512VLL16 datasheet supply voltage is 2.7V to 5.5V, so the question is if we use 3.3V as supply then is it okay for all operations, or else do we need to connect the 5V power supply.
 
Kindly check and suggest which supply is better for controller performance 3.3V or 5V?
0 项奖励
回复

5,397 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @prathamesh_h_patil ,

Either 3.3v or 5v is okey. You can freely determine VDD according to peripheral circuit. There is no difference in performance.

Regards,

Jing

0 项奖励
回复

5,386 次查看
prathamesh_h_patil
Contributor I

Dear NXP team,

If my supply of the controller is 3.3V then can I connect the 5V peripheral signal to controller and Vice versa?

Please confirm it.

 

Regards,

Prathamesh Patil

0 项奖励
回复

5,377 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @prathamesh_h_patil ,

No, you'd better don't design like that.

 

Regards,

Jing

0 项奖励
回复