Can MK24FN1M0VLL12 Support External SDRAM/SRAM & Flash ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can MK24FN1M0VLL12 Support External SDRAM/SRAM & Flash ?

ソリューションへジャンプ
2,473件の閲覧回数
pratik_panchal
Contributor II

I want to interface external SDRAM/SRAM & Flash with MK24FN1M0VLL12. is it possible or not?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,364件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Pratik,

    MK24FN1M0VLL12 can support the external flash with flexbus, but it can't support the external SDRAM, because it doesn't have the DDR module or the SDRAM module.

  But you want to use both the external flash and external SDRAM, you also can consider to use the MK26 series:

MK26FN2M0CAC18R
MK26FN2M0VLQ18
MK26FN2M0VMD18
MK26FN2M0VMI18

 The above MK26 chip can support both the flexbus and the SDRAM.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,365件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Pratik,

    MK24FN1M0VLL12 can support the external flash with flexbus, but it can't support the external SDRAM, because it doesn't have the DDR module or the SDRAM module.

  But you want to use both the external flash and external SDRAM, you also can consider to use the MK26 series:

MK26FN2M0CAC18R
MK26FN2M0VLQ18
MK26FN2M0VMD18
MK26FN2M0VMI18

 The above MK26 chip can support both the flexbus and the SDRAM.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,364件の閲覧回数
pratik_panchal
Contributor II

Thanks, Kerry Zhou,

Is there any other MCU series besides K26 series which can support external SDRAM and Flash?

How can I calculate the maximum supported external SDRAM/SRAM & Flash memory can be interfaced?

0 件の賞賛
返信