Can Kinetis I2S do "DSP Mode"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can Kinetis I2S do "DSP Mode"

ソリューションへジャンプ
2,029件の閲覧回数
CiaranMacA_hkc
Contributor III

Hi All,

I need to interface to a GSM modem which has an I2S audio interface - but the device implements "DSP Mode" only. That is to say, it uses an additional clock cycle to pulse the frame sync, then the following 16 cycles are used to clock the data. The interface does not toggle the Left / Right bit like standard I2S.

Thanks,

All the best,

CiaránDSP_ModeI2S.JPG

タグ(3)
0 件の賞賛
返信
1 解決策
1,608件の閲覧回数
CiaranMacA_hkc
Contributor III

In fact the answer is "Yes it can". I needed to configure my modem in Master mode and my I2S in "normal mode" with the tx and rx clocks (bit clk and frame sync) set to "external". Also needed to set the frame sync to 1 bit. A bit of trial and error on word format, alignment and so on and now it works superbly.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,609件の閲覧回数
CiaranMacA_hkc
Contributor III

In fact the answer is "Yes it can". I needed to configure my modem in Master mode and my I2S in "normal mode" with the tx and rx clocks (bit clk and frame sync) set to "external". Also needed to set the frame sync to 1 bit. A bit of trial and error on word format, alignment and so on and now it works superbly.

0 件の賞賛
返信