Can I write to Program Once IFR with an external device?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I write to Program Once IFR with an external device?

ソリューションへジャンプ
4,954件の閲覧回数
atilla
Contributor II

During production, we would like to write serial numbers to the program once field using the SWD connector (or maybe via ezPort?) How do we go about doing that? Is it possible with a PEMicro Cyclone? I think we need an algorithm to access the FCCOB registers.

ラベル(2)
0 件の賞賛
返信
1 解決策
4,773件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The OTP memory can't be programmed via EzPort.
It can be programmed via Jtag/SWD, however the controlling device needs to load a program to do it into SRAM (as it needs to do to program Flash). I see no reference to the PEMicro Cyclone programming tools supporting this but it is possible if the tools are give the capability - you should contact PEMicro to ask specifically.

Regards

Mark

元の投稿で解決策を見る

4 返答(返信)
4,773件の閲覧回数
johnny_pe
Contributor III

Hi Atilla,

Which Kinetis microcontroller are you working with?

Regards,
Johnny

PEMicro Support

0 件の賞賛
返信
4,773件の閲覧回数
atilla
Contributor II

I am using MK64FX512VLL12. Being able to program the PFLASH and DLFASH IFRs will sure come in handy for production.

0 件の賞賛
返信
4,773件の閲覧回数
johnny_pe
Contributor III

Hi Atilla,

Please open a support request on our website. We'll look into adding support for the PFLASH and DFLASH IFRs into our algorithm for the MK64FX512VLL12

www.pemicro.com

Regards,

Johnny

PEMicro Support

0 件の賞賛
返信
4,774件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The OTP memory can't be programmed via EzPort.
It can be programmed via Jtag/SWD, however the controlling device needs to load a program to do it into SRAM (as it needs to do to program Flash). I see no reference to the PEMicro Cyclone programming tools supporting this but it is possible if the tools are give the capability - you should contact PEMicro to ask specifically.

Regards

Mark