Can I write to Program Once IFR with an external device?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can I write to Program Once IFR with an external device?

跳至解决方案
3,196 次查看
atilla
Contributor II

During production, we would like to write serial numbers to the program once field using the SWD connector (or maybe via ezPort?) How do we go about doing that? Is it possible with a PEMicro Cyclone? I think we need an algorithm to access the FCCOB registers.

0 项奖励
回复
1 解答
3,016 次查看
mjbcswitzerland
Specialist V

Hi

The OTP memory can't be programmed via EzPort.
It can be programmed via Jtag/SWD, however the controlling device needs to load a program to do it into SRAM (as it needs to do to program Flash). I see no reference to the PEMicro Cyclone programming tools supporting this but it is possible if the tools are give the capability - you should contact PEMicro to ask specifically.

Regards

Mark

在原帖中查看解决方案

4 回复数
3,016 次查看
johnny_pe
Contributor III

Hi Atilla,

Which Kinetis microcontroller are you working with?

Regards,
Johnny

PEMicro Support

0 项奖励
回复
3,016 次查看
atilla
Contributor II

I am using MK64FX512VLL12. Being able to program the PFLASH and DLFASH IFRs will sure come in handy for production.

0 项奖励
回复
3,016 次查看
johnny_pe
Contributor III

Hi Atilla,

Please open a support request on our website. We'll look into adding support for the PFLASH and DFLASH IFRs into our algorithm for the MK64FX512VLL12

www.pemicro.com

Regards,

Johnny

PEMicro Support

0 项奖励
回复
3,017 次查看
mjbcswitzerland
Specialist V

Hi

The OTP memory can't be programmed via EzPort.
It can be programmed via Jtag/SWD, however the controlling device needs to load a program to do it into SRAM (as it needs to do to program Flash). I see no reference to the PEMicro Cyclone programming tools supporting this but it is possible if the tools are give the capability - you should contact PEMicro to ask specifically.

Regards

Mark